<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 PN5180 Dynamic Power Adjustment -&amp;gt; Make maximum</title>
    <link>https://community.nxp.com/t5/NXP-Designs/PN5180-Dynamic-Power-Adjustment-gt-Make-maximum/m-p/1037208#M377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to output maximum power with the NFC reader on the PN5180 board. It currently specifies that it will adjust its power output according to the proximity of the tag (lower power with closer proximity), but I want to maximize it to always output full power, or even more than it does by default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used the software to tune according to the distance (I can find that doc if need be), but it didn't mention how to maximize. Could I get some guidance here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Mar 2020 19:04:56 GMT</pubDate>
    <dc:creator>riley_baird</dc:creator>
    <dc:date>2020-03-02T19:04:56Z</dc:date>
    <item>
      <title>PN5180 Dynamic Power Adjustment -&gt; Make maximum</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-Dynamic-Power-Adjustment-gt-Make-maximum/m-p/1037208#M377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to output maximum power with the NFC reader on the PN5180 board. It currently specifies that it will adjust its power output according to the proximity of the tag (lower power with closer proximity), but I want to maximize it to always output full power, or even more than it does by default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used the software to tune according to the distance (I can find that doc if need be), but it didn't mention how to maximize. Could I get some guidance here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2020 19:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-Dynamic-Power-Adjustment-gt-Make-maximum/m-p/1037208#M377</guid>
      <dc:creator>riley_baird</dc:creator>
      <dc:date>2020-03-02T19:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Dynamic Power Adjustment -&gt; Make maximum</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-Dynamic-Power-Adjustment-gt-Make-maximum/m-p/1037209#M378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Hope you are doing great, please check the&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11742.pdf" title="https://www.nxp.com/docs/en/application-note/AN11742.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11742.pdf&lt;/A&gt;&amp;nbsp;&amp;nbsp;, section 1.2.1.1&amp;nbsp; you can find a note where it explains how to set the DPC&amp;nbsp; to one gear so it works the way you want.&lt;/P&gt;&lt;P&gt;Have a great day !&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2020 14:35:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-Dynamic-Power-Adjustment-gt-Make-maximum/m-p/1037209#M378</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-03-04T14:35:12Z</dc:date>
    </item>
  </channel>
</rss>