<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックExplore NFC Board support for Raspberry Pi 4</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Explore-NFC-Board-support-for-Raspberry-Pi-4/m-p/1006551#M270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a question about the product EXPLORE NFC Board for Raspberry Pi.&lt;/P&gt;&lt;P&gt;Does this board support the usage with the Raspberry Pi 4?&lt;/P&gt;&lt;P&gt;Because I am having some troubles with the linked NFC Reader Library for Linux V4&lt;/P&gt;&lt;P&gt;I am able to start the examples but e.g the Basic Discovery Loop does not return anything if an NFC Tag touches the Reader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Dec 2019 16:16:51 GMT</pubDate>
    <dc:creator>jakob1524</dc:creator>
    <dc:date>2019-12-04T16:16:51Z</dc:date>
    <item>
      <title>Explore NFC Board support for Raspberry Pi 4</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Explore-NFC-Board-support-for-Raspberry-Pi-4/m-p/1006551#M270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a question about the product EXPLORE NFC Board for Raspberry Pi.&lt;/P&gt;&lt;P&gt;Does this board support the usage with the Raspberry Pi 4?&lt;/P&gt;&lt;P&gt;Because I am having some troubles with the linked NFC Reader Library for Linux V4&lt;/P&gt;&lt;P&gt;I am able to start the examples but e.g the Basic Discovery Loop does not return anything if an NFC Tag touches the Reader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 16:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Explore-NFC-Board-support-for-Raspberry-Pi-4/m-p/1006551#M270</guid>
      <dc:creator>jakob1524</dc:creator>
      <dc:date>2019-12-04T16:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: Explore NFC Board support for Raspberry Pi 4</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Explore-NFC-Board-support-for-Raspberry-Pi-4/m-p/1006552#M271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far, just the SPI protocol is supported for the communication between reader IC and the Raspberry Pi, would you please check if the spi port has been set up correctly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.sudo raspi-config .&lt;BR /&gt;2.Advanced Options →SPI&lt;SPAN&gt;→&lt;/SPAN&gt;&amp;lt;Yes&amp;gt;&lt;BR /&gt;3.sudo reboot .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2019 05:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Explore-NFC-Board-support-for-Raspberry-Pi-4/m-p/1006552#M271</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-12-10T05:45:58Z</dc:date>
    </item>
  </channel>
</rss>