<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックHelp with ADC1 COCO</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Help-with-ADC1-COCO/m-p/916816#M16</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing a product with the MK20DX256VLL10. I am trying to get the A2D (both A2D0 and A2D1) to be controlled by either the PDB or LPTMR. I am also using DMA to switch inputs and restart A2D. I found a project K64F_ADC_DMA_Demo which has been helpful. This project uses A2D0, and the following:&lt;/P&gt;&lt;P&gt;DMAMUX_SetSource(DMAMUX0, DMAChannel_1, 40); /* Channel 1 Source 40: ADC COCO trigger */&lt;/P&gt;&lt;P&gt;sets up the DMA to start the A2D when ADC0 COCO. In this example, ADC0 COCO is "40". I want to perform the same operation using A2D1. I have not found what to put in the source for ADC1 COCO (replacing "40"). It has been very difficult to find documentation on this.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Sep 2019 12:48:23 GMT</pubDate>
    <dc:creator>pmasanek1</dc:creator>
    <dc:date>2019-09-26T12:48:23Z</dc:date>
    <item>
      <title>Help with ADC1 COCO</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Help-with-ADC1-COCO/m-p/916816#M16</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing a product with the MK20DX256VLL10. I am trying to get the A2D (both A2D0 and A2D1) to be controlled by either the PDB or LPTMR. I am also using DMA to switch inputs and restart A2D. I found a project K64F_ADC_DMA_Demo which has been helpful. This project uses A2D0, and the following:&lt;/P&gt;&lt;P&gt;DMAMUX_SetSource(DMAMUX0, DMAChannel_1, 40); /* Channel 1 Source 40: ADC COCO trigger */&lt;/P&gt;&lt;P&gt;sets up the DMA to start the A2D when ADC0 COCO. In this example, ADC0 COCO is "40". I want to perform the same operation using A2D1. I have not found what to put in the source for ADC1 COCO (replacing "40"). It has been very difficult to find documentation on this.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 12:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Help-with-ADC1-COCO/m-p/916816#M16</guid>
      <dc:creator>pmasanek1</dc:creator>
      <dc:date>2019-09-26T12:48:23Z</dc:date>
    </item>
    <item>
      <title>Re: Help with ADC1 COCO</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Help-with-ADC1-COCO/m-p/916817#M17</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following section in the reference manual:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3.3.9.1 DMA MUX request sources &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you could find the information you need here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 23:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Help-with-ADC1-COCO/m-p/916817#M17</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-10-01T23:01:47Z</dc:date>
    </item>
  </channel>
</rss>