<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックRe: PN7462 vcom doesnt show up after flashing Flash.bin/EEPROM.bin</title>
    <link>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992501#M158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved !!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mass area wasn`t soldered so the microcontroller was able to communicate only through the swd interface. But it didn`t function after the flash.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Dec 2019 08:46:16 GMT</pubDate>
    <dc:creator>raphael_werner</dc:creator>
    <dc:date>2019-12-09T08:46:16Z</dc:date>
    <item>
      <title>PN7462 vcom doesnt show up after flashing Flash.bin/EEPROM.bin</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992498#M155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guys&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After flashing my device over the mass storage it doesnt show up on the pc. &amp;nbsp;&lt;/P&gt;&lt;P&gt;I also have an evalboard but there is no Problem with the connection and the Vcom on the desktop.&lt;/P&gt;&lt;P&gt;Do I have to install another file to get it running.&lt;/P&gt;&lt;P&gt;Because I dont think that it is a Hardware Problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;gt; Windows 10&lt;/P&gt;&lt;P&gt;&lt;IMG /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yurs faithfully&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Raphael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2019 15:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992498#M155</guid>
      <dc:creator>raphael_werner</dc:creator>
      <dc:date>2019-12-02T15:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 vcom doesnt show up after flashing Flash.bin/EEPROM.bin</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992499#M156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Please refer to the more information as the&amp;nbsp; chapter 4.3&amp;nbsp;of UM10883.&amp;nbsp;&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/UM10883.pdf" title="https://www.nxp.com/docs/en/user-guide/UM10883.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM10883.pdf&lt;/A&gt;&amp;nbsp;. Hope it help you. Have a nice day.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 02:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992499#M156</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2019-12-04T02:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 vcom doesnt show up after flashing Flash.bin/EEPROM.bin</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992500#M157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello fangfang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chapter 5.3 (4.3) does not help me in the slightest because I am already able to Flash the PN7462.&lt;/P&gt;&lt;P&gt;The only Problem is that i can´t see the vCom on the PC after the flashing the two files "Flash &amp;amp; EEPROM" just as the evalboard.&lt;/P&gt;&lt;P&gt;I already checked the voltages and the Connections compared to the evalboard PNEV7462C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the PN7462AUHN and the following files:&lt;/P&gt;&lt;P&gt;….03_04_00_Flash.bin&lt;/P&gt;&lt;P&gt;….28_00_00_EEPROM.bin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 06:22:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992500#M157</guid>
      <dc:creator>raphael_werner</dc:creator>
      <dc:date>2019-12-04T06:22:41Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 vcom doesnt show up after flashing Flash.bin/EEPROM.bin</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992501#M158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved !!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mass area wasn`t soldered so the microcontroller was able to communicate only through the swd interface. But it didn`t function after the flash.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 08:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN7462-vcom-doesnt-show-up-after-flashing-Flash-bin-EEPROM-bin/m-p/992501#M158</guid>
      <dc:creator>raphael_werner</dc:creator>
      <dc:date>2019-12-09T08:46:16Z</dc:date>
    </item>
  </channel>
</rss>