<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックMRFX035H S-Parameters</title>
    <link>https://community.nxp.com/t5/NXP-Designs/MRFX035H-S-Parameters/m-p/2162699#M1206</link>
    <description>&lt;P&gt;I have a question regarding the S-parameters provided for the MRFX035:&lt;/P&gt;&lt;P&gt;I had used the S-paramters to match the MRFX035H to 300 MHz, but when I use the resulting circuit in real life, the matching is completely off. Are the S-Parameters provided on the web-page actually correct?&lt;/P&gt;&lt;P&gt;When I simulate the 230MHz reference board from the Datasheet using the S-parameters, the results show that it is matched for ~300 MHz. So something seems to be wrong there.&lt;/P&gt;&lt;P&gt;I'm using this file:&lt;/P&gt;&lt;P&gt;! 12/17/2018&lt;BR /&gt;! Rev 0&lt;BR /&gt;! MRFX035H S-Parameters&lt;BR /&gt;! Vdd=65V, IDQ=150mA&lt;/P&gt;</description>
    <pubDate>Wed, 03 Sep 2025 07:45:45 GMT</pubDate>
    <dc:creator>Stephan_Orzada</dc:creator>
    <dc:date>2025-09-03T07:45:45Z</dc:date>
    <item>
      <title>MRFX035H S-Parameters</title>
      <link>https://community.nxp.com/t5/NXP-Designs/MRFX035H-S-Parameters/m-p/2162699#M1206</link>
      <description>&lt;P&gt;I have a question regarding the S-parameters provided for the MRFX035:&lt;/P&gt;&lt;P&gt;I had used the S-paramters to match the MRFX035H to 300 MHz, but when I use the resulting circuit in real life, the matching is completely off. Are the S-Parameters provided on the web-page actually correct?&lt;/P&gt;&lt;P&gt;When I simulate the 230MHz reference board from the Datasheet using the S-parameters, the results show that it is matched for ~300 MHz. So something seems to be wrong there.&lt;/P&gt;&lt;P&gt;I'm using this file:&lt;/P&gt;&lt;P&gt;! 12/17/2018&lt;BR /&gt;! Rev 0&lt;BR /&gt;! MRFX035H S-Parameters&lt;BR /&gt;! Vdd=65V, IDQ=150mA&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 07:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/MRFX035H-S-Parameters/m-p/2162699#M1206</guid>
      <dc:creator>Stephan_Orzada</dc:creator>
      <dc:date>2025-09-03T07:45:45Z</dc:date>
    </item>
  </channel>
</rss>