<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM in NXP Designs</title>
    <link>https://community.nxp.com/t5/NXP-Designs/FRDM/m-p/2033906#M1186</link>
    <description>&lt;P&gt;I am starting a new project and I need advice as to which device to use.The requirements are quite simple. I need to control a heater using an i-phone (or similar) over the internet. The CPU needs to have a real-time-clock, at least one A/D or comparator and approx. 25 GPIO pins. My last design was with ai Kinetis device using MCUXpress. Which is the best device, do I need to use MCUXpress (already installed) or Virtual studio and is a development/debugger board available?&lt;/P&gt;</description>
    <pubDate>Fri, 24 Jan 2025 13:42:23 GMT</pubDate>
    <dc:creator>Julian99</dc:creator>
    <dc:date>2025-01-24T13:42:23Z</dc:date>
    <item>
      <title>FRDM</title>
      <link>https://community.nxp.com/t5/NXP-Designs/FRDM/m-p/2033906#M1186</link>
      <description>&lt;P&gt;I am starting a new project and I need advice as to which device to use.The requirements are quite simple. I need to control a heater using an i-phone (or similar) over the internet. The CPU needs to have a real-time-clock, at least one A/D or comparator and approx. 25 GPIO pins. My last design was with ai Kinetis device using MCUXpress. Which is the best device, do I need to use MCUXpress (already installed) or Virtual studio and is a development/debugger board available?&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jan 2025 13:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/FRDM/m-p/2033906#M1186</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2025-01-24T13:42:23Z</dc:date>
    </item>
  </channel>
</rss>