<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 TJA1102 remote WKU/LPS forwarding</title>
    <link>https://community.nxp.com/t5/NXP-Designs/TJA1102-remote-WKU-LPS-forwarding/m-p/1973618#M1166</link>
    <description>&lt;P&gt;Hi!&lt;BR /&gt;&lt;BR /&gt;Following situation:&lt;BR /&gt;- Two automotive eth (&lt;STRONG&gt;E1&lt;/STRONG&gt; and &lt;STRONG&gt;E2&lt;/STRONG&gt;) are in communication&lt;BR /&gt;- To sniff the traffic device with TJA1102 dual PHY is inserted in between&lt;BR /&gt;- The phy works in RMII_mode = "10",&amp;nbsp; RMII mode enabled (25 MHz XTAL output on Px_REF_CLK) and reverse mii mode is also an option (&amp;nbsp;RMII_mode = "11" )&lt;BR /&gt;- The traffic sent from "&lt;STRONG&gt;E1&lt;/STRONG&gt;" arrives on the &lt;STRONG&gt;PHY A&lt;/STRONG&gt; of TJA1102, it isforwarded to a &lt;STRONG&gt;PHY B&lt;/STRONG&gt; placed in the same TJA1102 package where from it is forwarded to the &lt;STRONG&gt;E2&lt;/STRONG&gt;.&lt;BR /&gt;- Problem arrives when I come to remote &lt;STRONG&gt;WAKE UP&lt;/STRONG&gt; and &lt;STRONG&gt;SLEEP&lt;/STRONG&gt; forwarding. If &lt;STRONG&gt;E1&lt;/STRONG&gt; sends &lt;STRONG&gt;WKU&lt;/STRONG&gt; request, I expect &lt;STRONG&gt;TJA1102 PHY A&lt;/STRONG&gt; to receive it, forward it to the &lt;STRONG&gt;PHY B&lt;/STRONG&gt;, which would send request (or pulses depending on the link status) to the &lt;STRONG&gt;E2&lt;/STRONG&gt;. TJA1102 should stay in normal power mode and should just forward the requests ....&lt;BR /&gt;To achieve this following register fields values are set:&lt;/P&gt;&lt;P&gt;- FWDPHYLOC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0 ( do not want request to have influence on the sniff device )&lt;BR /&gt;- REMWUPHY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 1&lt;BR /&gt;- LOCWUPHY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0 ( not using local wku/sleep at the moment)&lt;BR /&gt;- SLEEP_CONFIRM = 1 ( E1 needs approval from E2 to go to SLEEP mode)&lt;BR /&gt;- LPS_WUR_DIS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0&lt;BR /&gt;- SLEEP_ACK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 1&lt;BR /&gt;- FWDPHYREM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 1&lt;BR /&gt;- LPS_ACTIVE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 1&lt;BR /&gt;&lt;BR /&gt;This is the config for both PHYs in TJA1102 package. I am expecting the requests to be passed from one PHY to the other one in the package internally ( I was expecting when the PHY is in reverse MII mode, working as a repeater,&amp;nbsp; it would work, but it does not. If E1 initiates the request it does not reach E2 (all interrupts are enabled, checking Remote_wakeUp and LPS_received register fields).&lt;BR /&gt;&lt;BR /&gt;Is there something I am missing here, or this should achieve in different way.&lt;BR /&gt;&lt;BR /&gt;Thank You very much,&lt;BR /&gt;Nebojsa&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 14 Oct 2024 21:22:12 GMT</pubDate>
    <dc:creator>Markovic</dc:creator>
    <dc:date>2024-10-14T21:22:12Z</dc:date>
    <item>
      <title>TJA1102 remote WKU/LPS forwarding</title>
      <link>https://community.nxp.com/t5/NXP-Designs/TJA1102-remote-WKU-LPS-forwarding/m-p/1973618#M1166</link>
      <description>&lt;P&gt;Hi!&lt;BR /&gt;&lt;BR /&gt;Following situation:&lt;BR /&gt;- Two automotive eth (&lt;STRONG&gt;E1&lt;/STRONG&gt; and &lt;STRONG&gt;E2&lt;/STRONG&gt;) are in communication&lt;BR /&gt;- To sniff the traffic device with TJA1102 dual PHY is inserted in between&lt;BR /&gt;- The phy works in RMII_mode = "10",&amp;nbsp; RMII mode enabled (25 MHz XTAL output on Px_REF_CLK) and reverse mii mode is also an option (&amp;nbsp;RMII_mode = "11" )&lt;BR /&gt;- The traffic sent from "&lt;STRONG&gt;E1&lt;/STRONG&gt;" arrives on the &lt;STRONG&gt;PHY A&lt;/STRONG&gt; of TJA1102, it isforwarded to a &lt;STRONG&gt;PHY B&lt;/STRONG&gt; placed in the same TJA1102 package where from it is forwarded to the &lt;STRONG&gt;E2&lt;/STRONG&gt;.&lt;BR /&gt;- Problem arrives when I come to remote &lt;STRONG&gt;WAKE UP&lt;/STRONG&gt; and &lt;STRONG&gt;SLEEP&lt;/STRONG&gt; forwarding. If &lt;STRONG&gt;E1&lt;/STRONG&gt; sends &lt;STRONG&gt;WKU&lt;/STRONG&gt; request, I expect &lt;STRONG&gt;TJA1102 PHY A&lt;/STRONG&gt; to receive it, forward it to the &lt;STRONG&gt;PHY B&lt;/STRONG&gt;, which would send request (or pulses depending on the link status) to the &lt;STRONG&gt;E2&lt;/STRONG&gt;. TJA1102 should stay in normal power mode and should just forward the requests ....&lt;BR /&gt;To achieve this following register fields values are set:&lt;/P&gt;&lt;P&gt;- FWDPHYLOC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0 ( do not want request to have influence on the sniff device )&lt;BR /&gt;- REMWUPHY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 1&lt;BR /&gt;- LOCWUPHY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0 ( not using local wku/sleep at the moment)&lt;BR /&gt;- SLEEP_CONFIRM = 1 ( E1 needs approval from E2 to go to SLEEP mode)&lt;BR /&gt;- LPS_WUR_DIS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0&lt;BR /&gt;- SLEEP_ACK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 1&lt;BR /&gt;- FWDPHYREM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; 1&lt;BR /&gt;- LPS_ACTIVE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 1&lt;BR /&gt;&lt;BR /&gt;This is the config for both PHYs in TJA1102 package. I am expecting the requests to be passed from one PHY to the other one in the package internally ( I was expecting when the PHY is in reverse MII mode, working as a repeater,&amp;nbsp; it would work, but it does not. If E1 initiates the request it does not reach E2 (all interrupts are enabled, checking Remote_wakeUp and LPS_received register fields).&lt;BR /&gt;&lt;BR /&gt;Is there something I am missing here, or this should achieve in different way.&lt;BR /&gt;&lt;BR /&gt;Thank You very much,&lt;BR /&gt;Nebojsa&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 21:22:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/TJA1102-remote-WKU-LPS-forwarding/m-p/1973618#M1166</guid>
      <dc:creator>Markovic</dc:creator>
      <dc:date>2024-10-14T21:22:12Z</dc:date>
    </item>
  </channel>
</rss>