<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 K64F with KW41Z module ?</title>
    <link>https://community.nxp.com/t5/NXP-Designs/K64F-with-KW41Z-module/m-p/1882532#M1142</link>
    <description>&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;I'm discovering Thread protocol and for the needs of my project, I would like to create a communication card that would be able to act as a border router. Going through NXP documentation, I found two possible implementation:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - i.MX6 UL as host processor, running Linux, and a radio module with KW41Z&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - K64F as processor, running RTOS, associated with a MCR20A&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can one of these implementation be certified through inheritance?&lt;/P&gt;&lt;P&gt;Should one use K64F with KW41Z module ?&lt;/P&gt;&lt;P&gt;What are the steps in order to acquire development software&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jun 2024 07:49:54 GMT</pubDate>
    <dc:creator>Titaniya</dc:creator>
    <dc:date>2024-06-06T07:49:54Z</dc:date>
    <item>
      <title>K64F with KW41Z module ?</title>
      <link>https://community.nxp.com/t5/NXP-Designs/K64F-with-KW41Z-module/m-p/1882532#M1142</link>
      <description>&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;I'm discovering Thread protocol and for the needs of my project, I would like to create a communication card that would be able to act as a border router. Going through NXP documentation, I found two possible implementation:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - i.MX6 UL as host processor, running Linux, and a radio module with KW41Z&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - K64F as processor, running RTOS, associated with a MCR20A&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can one of these implementation be certified through inheritance?&lt;/P&gt;&lt;P&gt;Should one use K64F with KW41Z module ?&lt;/P&gt;&lt;P&gt;What are the steps in order to acquire development software&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 07:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/K64F-with-KW41Z-module/m-p/1882532#M1142</guid>
      <dc:creator>Titaniya</dc:creator>
      <dc:date>2024-06-06T07:49:54Z</dc:date>
    </item>
  </channel>
</rss>