<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Build Layerscape LDP image (ls1088ardb-pb) using bitbake (yocto) in NXP Designs</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Build-Layerscape-LDP-image-ls1088ardb-pb-using-bitbake-yocto/m-p/1875414#M1138</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When i build image for ls1088ardb-pb using bitbake i faced below error.&lt;BR /&gt;how to solve it&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;bitbake ls-image-lite&lt;/P&gt;&lt;P&gt;ERROR: linux-qoriq-6.1.y+gitAUTOINC+66e442bc7f-r0 do_assemble_fitimage_initramfs: Could not find a valid initramfs type for core-image-minimal-ls1088ardb-pb, the supported types are: cpio.lz4 cpio.lzo cpio.lzma cpio.xz cpio.zst cpio.gz ext2.gz cpio&lt;BR /&gt;ERROR: linux-qoriq-6.1.y+gitAUTOINC+66e442bc7f-r0 do_assemble_fitimage_initramfs: ExecutionError('/home/wilburl/NXP/yocto/build_ls1088ardb-pb/tmp/work/ls1088ardb_pb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/temp/run.do_assemble_fitimage_initramfs.2619713', 1, None, None)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/wilburl/NXP/yocto/build_ls1088ardb-pb/tmp/work/ls1088ardb_pb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/temp/log.do_assemble_fitimage_initramfs.2619713&lt;BR /&gt;ERROR: Task (/home/wilburl/NXP/yocto/sources/meta-qoriq/recipes-kernel/linux/linux-qoriq_6.1.bb:do_assemble_fitimage_initramfs) failed with exit code '1'&lt;/P&gt;</description>
    <pubDate>Mon, 27 May 2024 08:55:21 GMT</pubDate>
    <dc:creator>Lini</dc:creator>
    <dc:date>2024-05-27T08:55:21Z</dc:date>
    <item>
      <title>Build Layerscape LDP image (ls1088ardb-pb) using bitbake (yocto)</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Build-Layerscape-LDP-image-ls1088ardb-pb-using-bitbake-yocto/m-p/1875414#M1138</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When i build image for ls1088ardb-pb using bitbake i faced below error.&lt;BR /&gt;how to solve it&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;bitbake ls-image-lite&lt;/P&gt;&lt;P&gt;ERROR: linux-qoriq-6.1.y+gitAUTOINC+66e442bc7f-r0 do_assemble_fitimage_initramfs: Could not find a valid initramfs type for core-image-minimal-ls1088ardb-pb, the supported types are: cpio.lz4 cpio.lzo cpio.lzma cpio.xz cpio.zst cpio.gz ext2.gz cpio&lt;BR /&gt;ERROR: linux-qoriq-6.1.y+gitAUTOINC+66e442bc7f-r0 do_assemble_fitimage_initramfs: ExecutionError('/home/wilburl/NXP/yocto/build_ls1088ardb-pb/tmp/work/ls1088ardb_pb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/temp/run.do_assemble_fitimage_initramfs.2619713', 1, None, None)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/wilburl/NXP/yocto/build_ls1088ardb-pb/tmp/work/ls1088ardb_pb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/temp/log.do_assemble_fitimage_initramfs.2619713&lt;BR /&gt;ERROR: Task (/home/wilburl/NXP/yocto/sources/meta-qoriq/recipes-kernel/linux/linux-qoriq_6.1.bb:do_assemble_fitimage_initramfs) failed with exit code '1'&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 08:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Build-Layerscape-LDP-image-ls1088ardb-pb-using-bitbake-yocto/m-p/1875414#M1138</guid>
      <dc:creator>Lini</dc:creator>
      <dc:date>2024-05-27T08:55:21Z</dc:date>
    </item>
    <item>
      <title>Re: Build Layerscape LDP image (ls1088ardb-pb) using bitbake (yocto)</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Build-Layerscape-LDP-image-ls1088ardb-pb-using-bitbake-yocto/m-p/1875899#M1139</link>
      <description>&lt;P&gt;When I build the LDP image for the LS1088ARDB, it works fine. However, when I try to build it for the LS1088ARDB-PB, I encounter an error. Should I make any changes to the conf/local.conf file or the ls-image-lite.bb file to resolve this issue?&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 03:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Build-Layerscape-LDP-image-ls1088ardb-pb-using-bitbake-yocto/m-p/1875899#M1139</guid>
      <dc:creator>Lini</dc:creator>
      <dc:date>2024-05-28T03:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: Build Layerscape LDP image (ls1088ardb-pb) using bitbake (yocto)</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Build-Layerscape-LDP-image-ls1088ardb-pb-using-bitbake-yocto/m-p/1877072#M1140</link>
      <description>&lt;P&gt;Please apply the attached patches.&lt;/P&gt;</description>
      <pubDate>Wed, 29 May 2024 09:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Build-Layerscape-LDP-image-ls1088ardb-pb-using-bitbake-yocto/m-p/1877072#M1140</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-29T09:00:51Z</dc:date>
    </item>
  </channel>
</rss>