<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eMMc for LS1088A design in NXP Designs</title>
    <link>https://community.nxp.com/t5/NXP-Designs/eMMc-for-LS1088A-design/m-p/1868650#M1135</link>
    <description>&lt;P&gt;The LS1088a eSDHC is compatible with the &lt;STRONG&gt;eMMC&lt;/STRONG&gt; system specification version 4.5. It supports SDR50 and &lt;STRONG&gt;eMMC&lt;/STRONG&gt; high speed HS200 mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The eMMC device should be compatible with the &lt;STRONG&gt;eMMC&lt;/STRONG&gt; system specification version 5.1. It also supports SDR50 and &lt;STRONG&gt;eMMC&lt;/STRONG&gt; high speed HS200 mode.&lt;/P&gt;</description>
    <pubDate>Mon, 20 May 2024 07:08:51 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2024-05-20T07:08:51Z</dc:date>
    <item>
      <title>eMMc for LS1088A design</title>
      <link>https://community.nxp.com/t5/NXP-Designs/eMMc-for-LS1088A-design/m-p/1867644#M1134</link>
      <description>&lt;P&gt;I am designing a schematic using the LS1088A solution.&lt;/P&gt;&lt;P&gt;Currently, the eMMC lines recommended by NXP all have EoL, we are looking for a solution to replace them.&lt;/P&gt;&lt;P&gt;What types of eMMC are compatible with the LS1088A chipset? Can NXP provide suitable eMMC electrical specifications or alternative eMMC part?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 04:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/eMMc-for-LS1088A-design/m-p/1867644#M1134</guid>
      <dc:creator>Giang</dc:creator>
      <dc:date>2024-05-17T04:26:17Z</dc:date>
    </item>
    <item>
      <title>Re: eMMc for LS1088A design</title>
      <link>https://community.nxp.com/t5/NXP-Designs/eMMc-for-LS1088A-design/m-p/1868650#M1135</link>
      <description>&lt;P&gt;The LS1088a eSDHC is compatible with the &lt;STRONG&gt;eMMC&lt;/STRONG&gt; system specification version 4.5. It supports SDR50 and &lt;STRONG&gt;eMMC&lt;/STRONG&gt; high speed HS200 mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The eMMC device should be compatible with the &lt;STRONG&gt;eMMC&lt;/STRONG&gt; system specification version 5.1. It also supports SDR50 and &lt;STRONG&gt;eMMC&lt;/STRONG&gt; high speed HS200 mode.&lt;/P&gt;</description>
      <pubDate>Mon, 20 May 2024 07:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/eMMc-for-LS1088A-design/m-p/1868650#M1135</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-20T07:08:51Z</dc:date>
    </item>
  </channel>
</rss>