<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 NXP ls1088ardb booting from sd card</title>
    <link>https://community.nxp.com/t5/NXP-Designs/NXP-ls1088ardb-booting-from-sd-card/m-p/1834331#M1117</link>
    <description>&lt;P&gt;NOTICE: UDIMM 18ADF2G72AZ-2G6E1&lt;BR /&gt;ERROR: Board parameters no match.&lt;BR /&gt;ERROR: Failed matching board timing.&lt;BR /&gt;ERROR: Found training error(s): 0x2100&lt;BR /&gt;ERROR: Error: Waiting for D_INIT timeout.&lt;BR /&gt;ERROR: Writing DDR register(s) failed&lt;BR /&gt;ERROR: Programing DDRC error&lt;BR /&gt;ERROR: DDR init failed.&lt;BR /&gt;NOTICE: Incorrect DRAM0 size is defined in platfor_def.h&lt;BR /&gt;ERROR: mmap_add_region_check() failed. error -22&lt;BR /&gt;ERROR: mmap_add_region_check() failed. error -22&lt;BR /&gt;NOTICE: BL2: v1.5(release):LSDK-20.12&lt;BR /&gt;NOTICE: BL2: Built : 04:35:28, Dec 11 2020&lt;BR /&gt;this is the output when I try to boot the ls1088ardb board using sd card. how to fix this error&lt;/P&gt;</description>
    <pubDate>Mon, 25 Mar 2024 07:26:19 GMT</pubDate>
    <dc:creator>Rusanya_T</dc:creator>
    <dc:date>2024-03-25T07:26:19Z</dc:date>
    <item>
      <title>NXP ls1088ardb booting from sd card</title>
      <link>https://community.nxp.com/t5/NXP-Designs/NXP-ls1088ardb-booting-from-sd-card/m-p/1834331#M1117</link>
      <description>&lt;P&gt;NOTICE: UDIMM 18ADF2G72AZ-2G6E1&lt;BR /&gt;ERROR: Board parameters no match.&lt;BR /&gt;ERROR: Failed matching board timing.&lt;BR /&gt;ERROR: Found training error(s): 0x2100&lt;BR /&gt;ERROR: Error: Waiting for D_INIT timeout.&lt;BR /&gt;ERROR: Writing DDR register(s) failed&lt;BR /&gt;ERROR: Programing DDRC error&lt;BR /&gt;ERROR: DDR init failed.&lt;BR /&gt;NOTICE: Incorrect DRAM0 size is defined in platfor_def.h&lt;BR /&gt;ERROR: mmap_add_region_check() failed. error -22&lt;BR /&gt;ERROR: mmap_add_region_check() failed. error -22&lt;BR /&gt;NOTICE: BL2: v1.5(release):LSDK-20.12&lt;BR /&gt;NOTICE: BL2: Built : 04:35:28, Dec 11 2020&lt;BR /&gt;this is the output when I try to boot the ls1088ardb board using sd card. how to fix this error&lt;/P&gt;</description>
      <pubDate>Mon, 25 Mar 2024 07:26:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/NXP-ls1088ardb-booting-from-sd-card/m-p/1834331#M1117</guid>
      <dc:creator>Rusanya_T</dc:creator>
      <dc:date>2024-03-25T07:26:19Z</dc:date>
    </item>
  </channel>
</rss>