<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 problem on boot the nxp using sd card</title>
    <link>https://community.nxp.com/t5/NXP-Designs/problem-on-boot-the-nxp-using-sd-card/m-p/1830277#M1116</link>
    <description>&lt;P&gt;after editing the ddr parameters on ddr_init.c file how can i upload it on sd card. is there any possibilities to do that?&lt;BR /&gt;if I can upload that can I upload that as a image file or any other formats?&lt;BR /&gt;and where i can copy this one on sd card.&lt;BR /&gt;&lt;BR /&gt;#nxp #sdboot&lt;/P&gt;</description>
    <pubDate>Mon, 18 Mar 2024 11:47:02 GMT</pubDate>
    <dc:creator>Rusanya_T</dc:creator>
    <dc:date>2024-03-18T11:47:02Z</dc:date>
    <item>
      <title>problem on boot the nxp using sd card</title>
      <link>https://community.nxp.com/t5/NXP-Designs/problem-on-boot-the-nxp-using-sd-card/m-p/1830277#M1116</link>
      <description>&lt;P&gt;after editing the ddr parameters on ddr_init.c file how can i upload it on sd card. is there any possibilities to do that?&lt;BR /&gt;if I can upload that can I upload that as a image file or any other formats?&lt;BR /&gt;and where i can copy this one on sd card.&lt;BR /&gt;&lt;BR /&gt;#nxp #sdboot&lt;/P&gt;</description>
      <pubDate>Mon, 18 Mar 2024 11:47:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/problem-on-boot-the-nxp-using-sd-card/m-p/1830277#M1116</guid>
      <dc:creator>Rusanya_T</dc:creator>
      <dc:date>2024-03-18T11:47:02Z</dc:date>
    </item>
  </channel>
</rss>