<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックIs NTM88's pressure inlet waterproof?</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Is-NTM88-s-pressure-inlet-waterproof/m-p/1683617#M1063</link>
    <description>&lt;P&gt;I wanted to know if NTM88 can work if water goes inside its pressure hole. because i am using it for Tire pressure monitoring of tractor tires and tractor tires have some amount of water filled into them, which will lead to water entering inside the IC. So will this damage the IC?&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jul 2023 04:42:35 GMT</pubDate>
    <dc:creator>ankit2631</dc:creator>
    <dc:date>2023-07-07T04:42:35Z</dc:date>
    <item>
      <title>Is NTM88's pressure inlet waterproof?</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Is-NTM88-s-pressure-inlet-waterproof/m-p/1683617#M1063</link>
      <description>&lt;P&gt;I wanted to know if NTM88 can work if water goes inside its pressure hole. because i am using it for Tire pressure monitoring of tractor tires and tractor tires have some amount of water filled into them, which will lead to water entering inside the IC. So will this damage the IC?&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 04:42:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Is-NTM88-s-pressure-inlet-waterproof/m-p/1683617#M1063</guid>
      <dc:creator>ankit2631</dc:creator>
      <dc:date>2023-07-07T04:42:35Z</dc:date>
    </item>
    <item>
      <title>Re: Is NTM88's pressure inlet waterproof?</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Is-NTM88-s-pressure-inlet-waterproof/m-p/1684585#M1064</link>
      <description>&lt;P&gt;If only the&amp;nbsp;&lt;SPAN&gt;water goes inside its pressure hole,there is no problem.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 07:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Is-NTM88-s-pressure-inlet-waterproof/m-p/1684585#M1064</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-07-10T07:22:42Z</dc:date>
    </item>
  </channel>
</rss>