<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 PTN3460 LVDS Bridge - Emulation Disabled</title>
    <link>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1677272#M1059</link>
    <description>&lt;P&gt;Does anybody have experience using the PTN3460 device with emulation mode disabled?&lt;/P&gt;&lt;P&gt;Trying to use this mode but cannot get any display on the panel. Have not verified EDID data being retrieved from the panel on the DDC bus yet.&lt;/P&gt;&lt;P&gt;Where does EDID data retrieved from a panel reside on the bridge device? Is it accessible or visible?&lt;/P&gt;&lt;P&gt;The only change made to the registers is to clear the 'Enable EDID emulation' bit in the&amp;nbsp;EDID ROM emulation control register.&lt;/P&gt;</description>
    <pubDate>Tue, 27 Jun 2023 22:04:03 GMT</pubDate>
    <dc:creator>pauldemet</dc:creator>
    <dc:date>2023-06-27T22:04:03Z</dc:date>
    <item>
      <title>PTN3460 LVDS Bridge - Emulation Disabled</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1677272#M1059</link>
      <description>&lt;P&gt;Does anybody have experience using the PTN3460 device with emulation mode disabled?&lt;/P&gt;&lt;P&gt;Trying to use this mode but cannot get any display on the panel. Have not verified EDID data being retrieved from the panel on the DDC bus yet.&lt;/P&gt;&lt;P&gt;Where does EDID data retrieved from a panel reside on the bridge device? Is it accessible or visible?&lt;/P&gt;&lt;P&gt;The only change made to the registers is to clear the 'Enable EDID emulation' bit in the&amp;nbsp;EDID ROM emulation control register.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jun 2023 22:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1677272#M1059</guid>
      <dc:creator>pauldemet</dc:creator>
      <dc:date>2023-06-27T22:04:03Z</dc:date>
    </item>
    <item>
      <title>Re: PTN3460 LVDS Bridge - Emulation Disabled</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1677626#M1060</link>
      <description>&lt;P&gt;Suggest you follow the app note attached from page8-PTN3460 is in EDID emulation off mode (Configuration register 0x84 bit 0&lt;BR /&gt;= 0)&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 07:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1677626#M1060</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-06-28T07:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: PTN3460 LVDS Bridge - Emulation Disabled</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1677931#M1061</link>
      <description>&lt;P&gt;I am already doing this as stated in the original message. Is this all that needs to be done?&lt;/P&gt;&lt;P&gt;Any debug hints would be helpful.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 14:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1677931#M1061</guid>
      <dc:creator>pauldemet</dc:creator>
      <dc:date>2023-06-28T14:10:04Z</dc:date>
    </item>
    <item>
      <title>Re: PTN3460 LVDS Bridge - Emulation Disabled</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1678116#M1062</link>
      <description>&lt;P&gt;I believe I got this working now. Needed to add the flash memory step found on page 10.&lt;/P&gt;&lt;P&gt;The flow diagram does not show any delay between emulation mode being disabled and the flash memory sequence. I would expect some kind of delay for the EDID table to be retrieved from the panel.&lt;/P&gt;&lt;P&gt;I added a 3 second delay but would like to know what is required?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 22:50:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1678116#M1062</guid>
      <dc:creator>pauldemet</dc:creator>
      <dc:date>2023-06-28T22:50:12Z</dc:date>
    </item>
    <item>
      <title>Re: PTN3460 LVDS Bridge - Emulation Disabled</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1709336#M1076</link>
      <description>&lt;P&gt;IS the EDID table read from the panel accessible? Can I read back the EDID table?&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 19:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PTN3460-LVDS-Bridge-Emulation-Disabled/m-p/1709336#M1076</guid>
      <dc:creator>pauldemet</dc:creator>
      <dc:date>2023-08-22T19:35:01Z</dc:date>
    </item>
  </channel>
</rss>