<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>The NXP Cup Technical Reports中的主题 MPC8309-Tower Board</title>
    <link>https://community.nxp.com/t5/The-NXP-Cup-Technical-Reports/MPC8309-Tower-Board/m-p/491132#M21</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone, i am using MPC8309 tower board and i am facing problems with High speed USB port.&lt;/P&gt;&lt;P&gt;When an High speed device is connected to ECHI Host controller there is an error of -71 as per USB standards it is Protocol error and device is unable to enumerate at all ,if i connect with any intermediate device ,such as full speed USB hub device connected to host controller of ehci and&amp;nbsp; High speed device connected to full speed Hub device gets enumerated and i can establish PPP on that device through this setup,but Network gets lost after few minutes (upto 5 to 6 mins maximum)and modem get hanged and NO AT commands will be working as Modem got hanged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please anyone can help me reply ....? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Apr 2016 06:19:10 GMT</pubDate>
    <dc:creator>ganjiaravind</dc:creator>
    <dc:date>2016-04-09T06:19:10Z</dc:date>
    <item>
      <title>MPC8309-Tower Board</title>
      <link>https://community.nxp.com/t5/The-NXP-Cup-Technical-Reports/MPC8309-Tower-Board/m-p/491132#M21</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone, i am using MPC8309 tower board and i am facing problems with High speed USB port.&lt;/P&gt;&lt;P&gt;When an High speed device is connected to ECHI Host controller there is an error of -71 as per USB standards it is Protocol error and device is unable to enumerate at all ,if i connect with any intermediate device ,such as full speed USB hub device connected to host controller of ehci and&amp;nbsp; High speed device connected to full speed Hub device gets enumerated and i can establish PPP on that device through this setup,but Network gets lost after few minutes (upto 5 to 6 mins maximum)and modem get hanged and NO AT commands will be working as Modem got hanged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please anyone can help me reply ....? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Apr 2016 06:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/The-NXP-Cup-Technical-Reports/MPC8309-Tower-Board/m-p/491132#M21</guid>
      <dc:creator>ganjiaravind</dc:creator>
      <dc:date>2016-04-09T06:19:10Z</dc:date>
    </item>
  </channel>
</rss>