<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5554 PAD Configuration Register in The NXP Cup Technical Reports</title>
    <link>https://community.nxp.com/t5/The-NXP-Cup-Technical-Reports/MPC5554-PAD-Configuration-Register/m-p/464744#M19</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using MPC5554 for my project application.&lt;/P&gt;&lt;P&gt;I am an hardware design engineer and I have question regarding usage of GPIOs with pad configuration register (PCR) that corresponds to set of pads (some control 1 and others more than 10).The pad Configuration registers determines the settings of those pads. For example GPIO [147:162] are controlled by same PCR.&lt;/P&gt;&lt;P&gt;Can I use pins from these GPIOs as few inputs and few outputs ??&lt;/P&gt;&lt;P&gt;If yes would like to know how we can configure inputs and outputs using single PCR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Suresh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Mar 2016 18:44:34 GMT</pubDate>
    <dc:creator>sureshboddi</dc:creator>
    <dc:date>2016-03-10T18:44:34Z</dc:date>
    <item>
      <title>MPC5554 PAD Configuration Register</title>
      <link>https://community.nxp.com/t5/The-NXP-Cup-Technical-Reports/MPC5554-PAD-Configuration-Register/m-p/464744#M19</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using MPC5554 for my project application.&lt;/P&gt;&lt;P&gt;I am an hardware design engineer and I have question regarding usage of GPIOs with pad configuration register (PCR) that corresponds to set of pads (some control 1 and others more than 10).The pad Configuration registers determines the settings of those pads. For example GPIO [147:162] are controlled by same PCR.&lt;/P&gt;&lt;P&gt;Can I use pins from these GPIOs as few inputs and few outputs ??&lt;/P&gt;&lt;P&gt;If yes would like to know how we can configure inputs and outputs using single PCR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Suresh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Mar 2016 18:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/The-NXP-Cup-Technical-Reports/MPC5554-PAD-Configuration-Register/m-p/464744#M19</guid>
      <dc:creator>sureshboddi</dc:creator>
      <dc:date>2016-03-10T18:44:34Z</dc:date>
    </item>
  </channel>
</rss>