<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: Non-functioning OM5569 NFC Explorer Board</title>
    <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615008#M995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have the same problem as Mr. Dino has, I downloaded the new bin you posted, and tried to flash with the FWUpdate_CLOUD_3700_F_Ver1_00_BuildVer1_40.exe but no way, it states that the file is not correct and that no device with correct id is connected. I tried also with the application on the phore to reflash it, but it states that there was an error during flash (Error during memory flash). How could I solve the problem? Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jan 2017 11:17:13 GMT</pubDate>
    <dc:creator>ulrick</dc:creator>
    <dc:date>2017-01-30T11:17:13Z</dc:date>
    <item>
      <title>Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/614998#M985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just purchased an OM5569/NT322ER NTAG I2C plus Explorer Kit and it doesn't seem to be working.&amp;nbsp; The identiv Cloud reader works fine and its light changes from green to amber when I put an NTAG device on it and Windows does indeed recognize both the reader and the NTAG device.&amp;nbsp; However, neither the Peek/Poke nor Windows Demo program recognize the tag or the Explorer Board itself, and the Explorer board does not power up.&amp;nbsp; The Explorer board's LCD display powers up but the Explorer board doesn't do anything if I connect it to a PC via the USB connector - though I understand from the user guide that the Explorer board is supposed to get its power via the energy harvesting function of the NFC tag.&amp;nbsp; The setup behaves the same way on two separate PCs running Windows 10.&amp;nbsp; Am I doing something incorrectly here, do I have a dead board, corrupt firmware, or something else?&amp;nbsp; Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Dino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 13:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/614998#M985</guid>
      <dc:creator>dinofarina</dc:creator>
      <dc:date>2016-10-07T13:00:37Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/614999#M986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you applied the solution as below?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3035i2D3E752E577E6904/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to&amp;nbsp;&lt;A class="link-titled" href="http://www.nxp.com/documents/user_manual/UM10967.pdf" title="http://www.nxp.com/documents/user_manual/UM10967.pdf"&gt;http://www.nxp.com/documents/user_manual/UM10967.pdf&lt;/A&gt;&amp;nbsp; for more details.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Oct 2016 03:22:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/614999#M986</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-10-09T03:22:26Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615000#M987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've followed those instructions on 2 separate PCs to no avail.&amp;nbsp; It sure looks to me like the firmware on the OM5569 microcontroller is either corrupt or not installed at all.&amp;nbsp; Anything else I should try before sending the kit back for a refund?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Dino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2016 12:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615000#M987</guid>
      <dc:creator>dinofarina</dc:creator>
      <dc:date>2016-10-11T12:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615001#M988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dino,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a SWD port on the OM5569/NT322ER NTAG I2C plus Explorer board, you may download the firmware directly , and the code can be fetched from &lt;A class="link-titled" href="http://cache.nxp.com/documents/software/SW3649.zip" title="http://cache.nxp.com/documents/software/SW3649.zip"&gt;http://cache.nxp.com/documents/software/SW3649.zip&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to request a refund, please kindly refer to &lt;A class="link-titled" href="http://www.nxp.com/support/sales-and-support/buy-direct/returns-and-warranty-information:WTBUY_DTD_RETURNS" title="http://www.nxp.com/support/sales-and-support/buy-direct/returns-and-warranty-information:WTBUY_DTD_RETURNS"&gt;Returns and Warranty Information|NXP&lt;/A&gt;&amp;nbsp; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 02:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615001#M988</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-10-12T02:47:19Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615002#M989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Kan Li.&amp;nbsp; I'll let you know if the MCU re-flashing fixes the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Dino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 12:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615002#M989</guid>
      <dc:creator>dinofarina</dc:creator>
      <dc:date>2016-10-12T12:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615003#M990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I downloaded and unzipped the file in your link but do not see any firmware in the package - it looks like all the executables and source code for the desktop applications but not for the microcontroller.&amp;nbsp; Could you please advise?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Dino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 13:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615003#M990</guid>
      <dc:creator>dinofarina</dc:creator>
      <dc:date>2016-10-12T13:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615004#M991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dino,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, that is my mistake. Please kindly refer to &lt;A class="link-titled" href="http://cache.nxp.com/documents/software/SW309111.zip" title="http://cache.nxp.com/documents/software/SW309111.zip"&gt;http://cache.nxp.com/documents/software/SW309111.zip&lt;/A&gt;&amp;nbsp; for details. The firmware is in NTAG_I2C_LED_Demo_LPC812_1.6.zip.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 02:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615004#M991</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-10-13T02:32:23Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615005#M992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any pre-built binaries I could use to flash the MCU with?&amp;nbsp; I don't have any tools set up to handle the LPC parts.&amp;nbsp; Otherwise, I'll send the setup back for a refund.&amp;nbsp; Very frustrating to be perfectly honest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Dino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 16:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615005#M992</guid>
      <dc:creator>dinofarina</dc:creator>
      <dc:date>2016-10-13T16:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615006#M993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dino,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to the attachment for details.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan Li&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Oct 2016 05:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615006#M993</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-10-14T05:56:52Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615007#M994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The problem with gpedit.msc is that it is not available in many versions of Windows7&amp;nbsp; (Home Premium, Home Basic and Starter) &lt;SPAN&gt;...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my case, the NFC iDentiv uTrust 3700F reader did not work with "NTAG I2C Demo" until I update the firmware&amp;nbsp;&lt;SPAN style="background-color: #ffffff; color: #545454; font-size: small;"&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/software/SW4044.zip" title="http://cache.nxp.com/documents/software/SW4044.zip"&gt;http://cache.nxp.com/documents/software/SW4044.zip&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;firmware dated 10/18/2016 !)... and now it works, but with bugs he seems. (Eg it only reads 992 bytes while the Android program reads 1928 bytes !).&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Nov 2016 20:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615007#M994</guid>
      <dc:creator>jlvern</dc:creator>
      <dc:date>2016-11-09T20:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615008#M995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have the same problem as Mr. Dino has, I downloaded the new bin you posted, and tried to flash with the FWUpdate_CLOUD_3700_F_Ver1_00_BuildVer1_40.exe but no way, it states that the file is not correct and that no device with correct id is connected. I tried also with the application on the phore to reflash it, but it states that there was an error during flash (Error during memory flash). How could I solve the problem? Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2017 11:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615008#M995</guid>
      <dc:creator>ulrick</dc:creator>
      <dc:date>2017-01-30T11:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: Non-functioning OM5569 NFC Explorer Board</title>
      <link>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615009#M996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same issue and have spent all day and night trying to get it to work. I received the first board with the LCD screen broken and the second device does not seem to be working either. I am having the same issue. the reader driver is installed and recognized by the PC. when I plug the ntag board in nothing is displayed on the LCD screen even when placed over the reader. The LCD screen back lights up. I am using the PC NTAG I2C Demo PC app and that does not seem to recognize the board either. The peek and poke Utility does recognize the board and a "*" character is displayed on the screen. I have also tried to re-flash the board using my&amp;nbsp; j-link Plus and that wasn't successful either as I received an error indicating the board refused the connection.&amp;nbsp; please help as this is getting to be very frustrating.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2020 02:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Non-functioning-OM5569-NFC-Explorer-Board/m-p/615009#M996</guid>
      <dc:creator>wael_hazin</dc:creator>
      <dc:date>2020-08-27T02:53:05Z</dc:date>
    </item>
  </channel>
</rss>