<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7150 Not Entering Standby</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-Not-Entering-Standby/m-p/1557990#M9861</link>
    <description>&lt;P&gt;NXP,&lt;/P&gt;&lt;P&gt;I'm working on a design using the PN7150 and I'm having a problem where some of my PN7150s seemingly don't enter Stand-By mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So far, I've narrowed down the issue to correlating with the software revision of the PN7150.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have 2 OM5578 dev boards, one that was populated with&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;2&lt;/STRONG&gt;, and a second OM5578 where I replaced the PN7150 with a&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt;.&amp;nbsp; The OM5578 with the&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;2&lt;/STRONG&gt; briefly draws ~5 mA when the enable pin is held high, then returns to ~20 uA.&amp;nbsp; However, the OM5578 with the PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt;, draws ~5 mA continuously when the enable pin is held high. The power profile of the OM5578 with&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;2&lt;/STRONG&gt; behaves as expected, where the current returns to ~20uA in between RF transmissions in discovery mode, but one with the&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt; only ever drops to ~5mA.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The host controllers for both OM5578 are running the exact same firmware, based of the MCUXpresso example code.&amp;nbsp; I've ensured&amp;nbsp;&lt;STRONG&gt;CORE_SET_POWER_MODE_CMD&lt;/STRONG&gt; is set to 0x01 (Standby Mode Enabled) in the host controller firmware.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any other settings required to enter standby mode on&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt; parts?&amp;nbsp; Do you have any ideas what could be causing the PN7150 to continuously draw 5mA?&lt;/P&gt;&lt;P&gt;Appreciate any help.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;</description>
    <pubDate>Tue, 22 Nov 2022 19:41:28 GMT</pubDate>
    <dc:creator>danielp1</dc:creator>
    <dc:date>2022-11-22T19:41:28Z</dc:date>
    <item>
      <title>PN7150 Not Entering Standby</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Not-Entering-Standby/m-p/1557990#M9861</link>
      <description>&lt;P&gt;NXP,&lt;/P&gt;&lt;P&gt;I'm working on a design using the PN7150 and I'm having a problem where some of my PN7150s seemingly don't enter Stand-By mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So far, I've narrowed down the issue to correlating with the software revision of the PN7150.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have 2 OM5578 dev boards, one that was populated with&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;2&lt;/STRONG&gt;, and a second OM5578 where I replaced the PN7150 with a&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt;.&amp;nbsp; The OM5578 with the&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;2&lt;/STRONG&gt; briefly draws ~5 mA when the enable pin is held high, then returns to ~20 uA.&amp;nbsp; However, the OM5578 with the PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt;, draws ~5 mA continuously when the enable pin is held high. The power profile of the OM5578 with&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;2&lt;/STRONG&gt; behaves as expected, where the current returns to ~20uA in between RF transmissions in discovery mode, but one with the&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt; only ever drops to ~5mA.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The host controllers for both OM5578 are running the exact same firmware, based of the MCUXpresso example code.&amp;nbsp; I've ensured&amp;nbsp;&lt;STRONG&gt;CORE_SET_POWER_MODE_CMD&lt;/STRONG&gt; is set to 0x01 (Standby Mode Enabled) in the host controller firmware.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any other settings required to enter standby mode on&amp;nbsp;PN7150B0HN/C1100&lt;STRONG&gt;6&lt;/STRONG&gt; parts?&amp;nbsp; Do you have any ideas what could be causing the PN7150 to continuously draw 5mA?&lt;/P&gt;&lt;P&gt;Appreciate any help.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 22 Nov 2022 19:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Not-Entering-Standby/m-p/1557990#M9861</guid>
      <dc:creator>danielp1</dc:creator>
      <dc:date>2022-11-22T19:41:28Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Not Entering Standby</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Not-Entering-Standby/m-p/2196695#M13751</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209124"&gt;@danielp1&lt;/a&gt;&amp;nbsp;, any finding you could&amp;nbsp; share as there are no responses here to learn about this issue?&amp;nbsp; Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 31 Oct 2025 13:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Not-Entering-Standby/m-p/2196695#M13751</guid>
      <dc:creator>vil</dc:creator>
      <dc:date>2025-10-31T13:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Not Entering Standby</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Not-Entering-Standby/m-p/2205925#M13820</link>
      <description>&lt;P&gt;Hello All,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;PN7150&amp;nbsp;Version &lt;STRONG&gt;C11006&lt;/STRONG&gt; unfortunately does not support "standby mode", as written in the Datasheet below.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_1-1763368157170.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365863i1B1F97CFACCD49E6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_1-1763368157170.png" alt="Tomas_Parizek_1-1763368157170.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;As this product is not recommended for new designs, there is no plan to fix it. Please consider PN7160 for future designs.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Nov 2025 08:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Not-Entering-Standby/m-p/2205925#M13820</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2025-11-17T08:31:04Z</dc:date>
    </item>
  </channel>
</rss>