<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックMultiple PN7150 reader on a single system</title>
    <link>https://community.nxp.com/t5/NFC/Multiple-PN7150-reader-on-a-single-system/m-p/1542787#M9790</link>
    <description>&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;we plan to use 4 NFC reader PN7150 in a project.&lt;/P&gt;&lt;P&gt;Even if it is possible to use more than one chip on the same bus setting a different address (I can set 4 different addresses), it is not clear to me if I need 4 separate GPIO for enable or if I can use a common enable GPIO, and of course 4 different IRQ line.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;Stefano.&lt;/P&gt;</description>
    <pubDate>Mon, 24 Oct 2022 14:54:38 GMT</pubDate>
    <dc:creator>SCordibella</dc:creator>
    <dc:date>2022-10-24T14:54:38Z</dc:date>
    <item>
      <title>Multiple PN7150 reader on a single system</title>
      <link>https://community.nxp.com/t5/NFC/Multiple-PN7150-reader-on-a-single-system/m-p/1542787#M9790</link>
      <description>&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;we plan to use 4 NFC reader PN7150 in a project.&lt;/P&gt;&lt;P&gt;Even if it is possible to use more than one chip on the same bus setting a different address (I can set 4 different addresses), it is not clear to me if I need 4 separate GPIO for enable or if I can use a common enable GPIO, and of course 4 different IRQ line.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;Stefano.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Oct 2022 14:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Multiple-PN7150-reader-on-a-single-system/m-p/1542787#M9790</guid>
      <dc:creator>SCordibella</dc:creator>
      <dc:date>2022-10-24T14:54:38Z</dc:date>
    </item>
  </channel>
</rss>