<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 PN532 doesn't respond on SamConfiguartion</title>
    <link>https://community.nxp.com/t5/NFC/PN532-doesn-t-respond-on-SamConfiguartion/m-p/1542257#M9785</link>
    <description>&lt;P&gt;Hello Everybody,&lt;BR /&gt;&lt;BR /&gt;I faced a problem in PN532 that after a long time (reading cards) PN532 hangs on and does not respond even to the first SamConfiguration command sent over SPI. After sending the Reset signal the situation also doesn't change.&amp;nbsp;PN532 may start working normally after some time or after power on/off.&lt;/P&gt;&lt;P&gt;The schematic is as AN10609_2 recommends. And two more details - the PCB is covered with polyurethane and when we open the potting with the 35 - 40 pins, PN532 starts working normally. Also, the VBAT voltage is in the 3.2 - 3.4 V range. Could potting or voltage range be an issue?&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KirillT_0-1666465177239.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/197761i801081FB8AF1A6BF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KirillT_0-1666465177239.png" alt="KirillT_0-1666465177239.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Kirill&lt;/P&gt;</description>
    <pubDate>Sat, 22 Oct 2022 19:10:42 GMT</pubDate>
    <dc:creator>KirillT</dc:creator>
    <dc:date>2022-10-22T19:10:42Z</dc:date>
    <item>
      <title>PN532 doesn't respond on SamConfiguartion</title>
      <link>https://community.nxp.com/t5/NFC/PN532-doesn-t-respond-on-SamConfiguartion/m-p/1542257#M9785</link>
      <description>&lt;P&gt;Hello Everybody,&lt;BR /&gt;&lt;BR /&gt;I faced a problem in PN532 that after a long time (reading cards) PN532 hangs on and does not respond even to the first SamConfiguration command sent over SPI. After sending the Reset signal the situation also doesn't change.&amp;nbsp;PN532 may start working normally after some time or after power on/off.&lt;/P&gt;&lt;P&gt;The schematic is as AN10609_2 recommends. And two more details - the PCB is covered with polyurethane and when we open the potting with the 35 - 40 pins, PN532 starts working normally. Also, the VBAT voltage is in the 3.2 - 3.4 V range. Could potting or voltage range be an issue?&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KirillT_0-1666465177239.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/197761i801081FB8AF1A6BF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KirillT_0-1666465177239.png" alt="KirillT_0-1666465177239.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Kirill&lt;/P&gt;</description>
      <pubDate>Sat, 22 Oct 2022 19:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN532-doesn-t-respond-on-SamConfiguartion/m-p/1542257#M9785</guid>
      <dc:creator>KirillT</dc:creator>
      <dc:date>2022-10-22T19:10:42Z</dc:date>
    </item>
  </channel>
</rss>