<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Capacitor rating for PN5190 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Capacitor-rating-for-PN5190/m-p/1533249#M9740</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to confirm the voltage rating for capacitors in matching network for PN5190 EVB (PNEV5190B).&lt;/P&gt;&lt;P&gt;The BOM in the design files is not fully detailed with commercial part numbers so I can not find compatible parts.&lt;/P&gt;&lt;P&gt;I think they are rated to 250V because a collegue could open the source altium file, but I need confirmation asap because we would like to use 0603/0402 instead of 0805.&lt;/P&gt;&lt;P&gt;One question:&lt;/P&gt;&lt;P&gt;Why do matching capacitors in CLEV6630B_V2.0 are rated to 50V&amp;nbsp;and 250V for PNEV5190B if both Front Ends are specified to have 2W?&lt;/P&gt;&lt;P&gt;Please, provide &lt;STRONG&gt;fulll detailed BOM for&amp;nbsp;PNEV5190B base board &lt;/STRONG&gt;at your earliest convininence.&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Oct 2022 08:26:14 GMT</pubDate>
    <dc:creator>jr_hernandez</dc:creator>
    <dc:date>2022-10-06T08:26:14Z</dc:date>
    <item>
      <title>Capacitor rating for PN5190</title>
      <link>https://community.nxp.com/t5/NFC/Capacitor-rating-for-PN5190/m-p/1533249#M9740</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to confirm the voltage rating for capacitors in matching network for PN5190 EVB (PNEV5190B).&lt;/P&gt;&lt;P&gt;The BOM in the design files is not fully detailed with commercial part numbers so I can not find compatible parts.&lt;/P&gt;&lt;P&gt;I think they are rated to 250V because a collegue could open the source altium file, but I need confirmation asap because we would like to use 0603/0402 instead of 0805.&lt;/P&gt;&lt;P&gt;One question:&lt;/P&gt;&lt;P&gt;Why do matching capacitors in CLEV6630B_V2.0 are rated to 50V&amp;nbsp;and 250V for PNEV5190B if both Front Ends are specified to have 2W?&lt;/P&gt;&lt;P&gt;Please, provide &lt;STRONG&gt;fulll detailed BOM for&amp;nbsp;PNEV5190B base board &lt;/STRONG&gt;at your earliest convininence.&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Oct 2022 08:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Capacitor-rating-for-PN5190/m-p/1533249#M9740</guid>
      <dc:creator>jr_hernandez</dc:creator>
      <dc:date>2022-10-06T08:26:14Z</dc:date>
    </item>
  </channel>
</rss>