<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN5190 NfCRdLib - Problems with NfcrdlibEx1_DiscoveryLoop in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN5190-NfCRdLib-Problems-with-NfcrdlibEx1-DiscoveryLoop/m-p/1529511#M9719</link>
    <description>&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;I have detected an issue in the SPI transfer when placing the card and the command EXCHANGE_RF_DATA is executed:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jr_hernandez_0-1664365397936.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195175i85445BA686DB4D0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="jr_hernandez_0-1664365397936.png" alt="jr_hernandez_0-1664365397936.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jr_hernandez_0-1664365397936.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;According to the TLV scheme the received frame is 0x0D = 13 bytes long, but only 9 are expected when SPI exchange is invoked. This length is set internally in the NfcLib, right?&lt;/P&gt;&lt;P&gt;Why is this happening?&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 28 Sep 2022 11:47:38 GMT</pubDate>
    <dc:creator>jr_hernandez</dc:creator>
    <dc:date>2022-09-28T11:47:38Z</dc:date>
    <item>
      <title>PN5190 NfCRdLib - Problems with NfcrdlibEx1_DiscoveryLoop</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-NfCRdLib-Problems-with-NfcrdlibEx1-DiscoveryLoop/m-p/1529481#M9718</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am facing some troubles when running the&amp;nbsp;NfcrdlibEx1_DiscoveryLoop example.&lt;/P&gt;&lt;P&gt;I have ported myself to ESP32 and using NullOs mode fo OS layer by now.&lt;/P&gt;&lt;P&gt;The P5190 seems to boot correctly and starts LPCD (see SPI frames below).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DiscoveryLoop Example:&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;-DEBUG-: [ 0,300 s] SPI WR &amp;gt;&amp;gt; 0x 7F 20 01 00&lt;BR /&gt;-DEBUG-: [ 0,319 s] SPI RD &amp;lt;&amp;lt; 0x FF 80 00 08&lt;BR /&gt;-DEBUG-: [ 0,338 s] SPI RD &amp;lt;&amp;lt; 0x FF 01 00 00 00 01 00 00 00&lt;/P&gt;&lt;P&gt;PN5190 Booted correctly&lt;/P&gt;&lt;P&gt;-DEBUG-: [ 0,353 s] phNfcLib_GetDataParams...&lt;BR /&gt;-DEBUG-: [ 0,390 s] SPI WR &amp;gt;&amp;gt; 0x 7F 06 00 1A B3 02 04 00 A1 A2 A3 40 01 FE B2 B3 B4 B5 B6 B7 C0 C1 C2 C3 C4 C5 C6 C7 23 45&lt;BR /&gt;-DEBUG-: [ 0,423 s] SPI RD &amp;lt;&amp;lt; 0x FF 06 00 01 00 FF FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,438 s] SPI WR &amp;gt;&amp;gt; 0x 7F 06 00 03 CB 02 01&lt;BR /&gt;-DEBUG-: [ 0,465 s] SPI RD &amp;lt;&amp;lt; 0x FF 06 00 01 00 FF FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,480 s] SPI WR &amp;gt;&amp;gt; 0x 7F 02 00 05 03 FE FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,508 s] SPI RD &amp;lt;&amp;lt; 0x FF 02 00 01 00 FF FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,523 s] SPI WR &amp;gt;&amp;gt; 0x 7F 11 00 00&lt;BR /&gt;-DEBUG-: [ 0,550 s] SPI RD &amp;lt;&amp;lt; 0x FF 11 00 01 00 FF FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,655 s] SPI WR &amp;gt;&amp;gt; 0x 7F 23 00 08 02 00 00 00 00 00 64 00&lt;BR /&gt;0x FF 23 00 01 00 FF FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,713 s] SPI RD &amp;lt;&amp;lt; 0x FF 80 00 08 00 02 00 00 E6&lt;BR /&gt;-DEBUG-: [ 0,738 s] SPI RD &amp;lt;&amp;lt; 0x FF FF C6 FF&lt;BR /&gt;-DEBUG-: [ 0,755 s] SPI WR &amp;gt;&amp;gt; 0x 7F 02 00 05 03 FE FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,782 s] SPI RD &amp;lt;&amp;lt; 0x FF 02 00 01 00 FF FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,798 s] SPI WR &amp;gt;&amp;gt; 0x 7F 02 00 05 08 F7 FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,825 s] SPI RD &amp;lt;&amp;lt; 0x FF 02 00 01 00 FF FF FF FF&lt;BR /&gt;-DEBUG-: [ 0,842 s] SPI WR &amp;gt;&amp;gt; 0x 7F 23 00 08 03 00 E6 FF C6 FF 4A 01&lt;BR /&gt;-DEBUG-: [ 0,871 s] SPI RD &amp;lt;&amp;lt; 0x FF 23 00 01 00 FF FF FF FF&lt;/P&gt;&lt;P&gt;But as soon as a card is placed on field it tries some active poll and nothing is reported.&lt;/P&gt;&lt;P&gt;It performs several SPI transfers and the remains with RF off.&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 10:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-NfCRdLib-Problems-with-NfcrdlibEx1-DiscoveryLoop/m-p/1529481#M9718</guid>
      <dc:creator>jr_hernandez</dc:creator>
      <dc:date>2022-09-28T10:23:11Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 NfCRdLib - Problems with NfcrdlibEx1_DiscoveryLoop</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-NfCRdLib-Problems-with-NfcrdlibEx1-DiscoveryLoop/m-p/1529511#M9719</link>
      <description>&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;I have detected an issue in the SPI transfer when placing the card and the command EXCHANGE_RF_DATA is executed:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jr_hernandez_0-1664365397936.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195175i85445BA686DB4D0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="jr_hernandez_0-1664365397936.png" alt="jr_hernandez_0-1664365397936.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jr_hernandez_0-1664365397936.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;According to the TLV scheme the received frame is 0x0D = 13 bytes long, but only 9 are expected when SPI exchange is invoked. This length is set internally in the NfcLib, right?&lt;/P&gt;&lt;P&gt;Why is this happening?&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 11:47:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-NfCRdLib-Problems-with-NfcrdlibEx1-DiscoveryLoop/m-p/1529511#M9719</guid>
      <dc:creator>jr_hernandez</dc:creator>
      <dc:date>2022-09-28T11:47:38Z</dc:date>
    </item>
  </channel>
</rss>