<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN5190 ULPCD</title>
    <link>https://community.nxp.com/t5/NFC/PN5190-ULPCD/m-p/1514489#M9626</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to test ULPCD for PN5190. I am using PNEV5190, but not sure how to set the power jumpers.&lt;/P&gt;&lt;P&gt;I do not want to damage the board.&lt;/P&gt;&lt;P&gt;As far as I have understood internal DC-DC must be disabled, my guess is to set jumper J13 to short 1-2 (so VUP is connected to 3V3).&lt;/P&gt;&lt;P&gt;Before setting the jumper I have set the ULPCD to the EEPROM, but there is still in 3,6v in VUP.&lt;/P&gt;&lt;P&gt;Any suggestions on how to setup the UPLCD?&lt;/P&gt;&lt;P&gt;Is there any guide with further details about the ULPCD?&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 31 Aug 2022 08:35:53 GMT</pubDate>
    <dc:creator>jr_hernandez</dc:creator>
    <dc:date>2022-08-31T08:35:53Z</dc:date>
    <item>
      <title>PN5190 ULPCD</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-ULPCD/m-p/1514489#M9626</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to test ULPCD for PN5190. I am using PNEV5190, but not sure how to set the power jumpers.&lt;/P&gt;&lt;P&gt;I do not want to damage the board.&lt;/P&gt;&lt;P&gt;As far as I have understood internal DC-DC must be disabled, my guess is to set jumper J13 to short 1-2 (so VUP is connected to 3V3).&lt;/P&gt;&lt;P&gt;Before setting the jumper I have set the ULPCD to the EEPROM, but there is still in 3,6v in VUP.&lt;/P&gt;&lt;P&gt;Any suggestions on how to setup the UPLCD?&lt;/P&gt;&lt;P&gt;Is there any guide with further details about the ULPCD?&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 08:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-ULPCD/m-p/1514489#M9626</guid>
      <dc:creator>jr_hernandez</dc:creator>
      <dc:date>2022-08-31T08:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 ULPCD</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-ULPCD/m-p/1514540#M9628</link>
      <description>&lt;P&gt;HI again,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems you need to press "Read HF attenuator" button in order to apply settings. Now, VUP is 1,4 V (residual voltage, I guess). After connecting the jumper as said above ULPCD is working.&lt;/P&gt;&lt;P&gt;See my results about detection range:&lt;/P&gt;&lt;P&gt;LPDC -&amp;gt; CARD (55 mm) PHONE (55 mm)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U&lt;/STRONG&gt;LPDC -&amp;gt; CARD (71 mm) PHONE (34 mm)&lt;/P&gt;&lt;P&gt;Is it normal that the detection range is larger with UPCD than with LPCD?&lt;/P&gt;&lt;P&gt;Why range is uniform across card/phone with LPCD and not with ULPCD?&lt;/P&gt;&lt;P&gt;Regards, Ramon.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Aug 2022 09:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-ULPCD/m-p/1514540#M9628</guid>
      <dc:creator>jr_hernandez</dc:creator>
      <dc:date>2022-08-31T09:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 ULPCD</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-ULPCD/m-p/1523458#M9674</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Due to the detuning effect there could be some differences, it is hard to judge the detection range.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 16 Sep 2022 07:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-ULPCD/m-p/1523458#M9674</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-09-16T07:23:46Z</dc:date>
    </item>
  </channel>
</rss>