<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7150 | issue while running Arduino library in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-issue-while-running-Arduino-library/m-p/1490614#M9561</link>
    <description>&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;My customer is using an Arduino type of device (actually the device calls Particle Photon-Zero).&lt;/P&gt;&lt;P&gt;he was trying to import the Arduino library for I2C access to the PN7150 NFC as a reader and he pick the&amp;nbsp;Electronic Cats PN7150.&lt;/P&gt;&lt;P&gt;somehow when he runs the library it failed on&amp;nbsp;CORE_CONF_EXTN.&lt;/P&gt;&lt;P&gt;after comparing the library code vs the Example code of NCI2 (from the LPC55 demo code), it looks okay but somehow when we send the CORE_CONF_EXTN configuration it fails (see below log):&lt;/P&gt;&lt;P&gt;Initializing...&lt;BR /&gt;0xROM_CODE_V: 10&lt;BR /&gt;FW_MAJOR_NO: 1&lt;BR /&gt;0xFW_MINOR_NO: a0&lt;BR /&gt;gNfcController_generation: 2&lt;BR /&gt;rxBuffer[0]: 0 rxBuffer[1]: 0 rxBuffer[3]: 0 rxBuffer[4]: 1&lt;BR /&gt;NxpNci_CORE_CONF_EXTN&lt;BR /&gt;The Configure Settings is failed!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;This is the expect response is as follow&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;STRONG&gt;if&lt;/STRONG&gt; ((Answer[0] != 0x40) || (Answer[1] != 0x02) || (Answer[3] != 0x00) || (Answer[4] != 0x00))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the customer response&lt;/P&gt;&lt;P&gt;rxBuffer[0]: 0 rxBuffer[1]: 0 rxBuffer[3]: 0 rxBuffer[4]: 1&lt;/P&gt;&lt;P&gt;Could you please advise back what could be the issue here?&lt;/P&gt;&lt;P&gt;Wating for your kind feedback, Many Thanks.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shai&lt;/P&gt;</description>
    <pubDate>Sun, 17 Jul 2022 14:37:46 GMT</pubDate>
    <dc:creator>shai_b</dc:creator>
    <dc:date>2022-07-17T14:37:46Z</dc:date>
    <item>
      <title>PN7150 | issue while running Arduino library</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-issue-while-running-Arduino-library/m-p/1490614#M9561</link>
      <description>&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;My customer is using an Arduino type of device (actually the device calls Particle Photon-Zero).&lt;/P&gt;&lt;P&gt;he was trying to import the Arduino library for I2C access to the PN7150 NFC as a reader and he pick the&amp;nbsp;Electronic Cats PN7150.&lt;/P&gt;&lt;P&gt;somehow when he runs the library it failed on&amp;nbsp;CORE_CONF_EXTN.&lt;/P&gt;&lt;P&gt;after comparing the library code vs the Example code of NCI2 (from the LPC55 demo code), it looks okay but somehow when we send the CORE_CONF_EXTN configuration it fails (see below log):&lt;/P&gt;&lt;P&gt;Initializing...&lt;BR /&gt;0xROM_CODE_V: 10&lt;BR /&gt;FW_MAJOR_NO: 1&lt;BR /&gt;0xFW_MINOR_NO: a0&lt;BR /&gt;gNfcController_generation: 2&lt;BR /&gt;rxBuffer[0]: 0 rxBuffer[1]: 0 rxBuffer[3]: 0 rxBuffer[4]: 1&lt;BR /&gt;NxpNci_CORE_CONF_EXTN&lt;BR /&gt;The Configure Settings is failed!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;This is the expect response is as follow&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;STRONG&gt;if&lt;/STRONG&gt; ((Answer[0] != 0x40) || (Answer[1] != 0x02) || (Answer[3] != 0x00) || (Answer[4] != 0x00))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the customer response&lt;/P&gt;&lt;P&gt;rxBuffer[0]: 0 rxBuffer[1]: 0 rxBuffer[3]: 0 rxBuffer[4]: 1&lt;/P&gt;&lt;P&gt;Could you please advise back what could be the issue here?&lt;/P&gt;&lt;P&gt;Wating for your kind feedback, Many Thanks.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shai&lt;/P&gt;</description>
      <pubDate>Sun, 17 Jul 2022 14:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-issue-while-running-Arduino-library/m-p/1490614#M9561</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2022-07-17T14:37:46Z</dc:date>
    </item>
  </channel>
</rss>