<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7160B - CPOL Configuration</title>
    <link>https://community.nxp.com/t5/NFC/PN7160B-CPOL-Configuration/m-p/1488716#M9548</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;As described in PN7160 Datasheet, 11.2.2.2 SPI-bus configuration options:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;In order to select SPI-bus interface for host communication, some EEPROM settings are&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;programmed during production.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Four versions can be configured depending on CPOL/CPHA EEPROM setting.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The selection between interfaces is fused during IC manufacturing so that different&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ordering numbers for the SPI-bus version.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I have not found any information on different ordernumbers that affect the settings.&lt;BR /&gt;Is this an error?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
    <pubDate>Wed, 13 Jul 2022 11:08:12 GMT</pubDate>
    <dc:creator>michael_d_1983</dc:creator>
    <dc:date>2022-07-13T11:08:12Z</dc:date>
    <item>
      <title>PN7160B - CPOL Configuration</title>
      <link>https://community.nxp.com/t5/NFC/PN7160B-CPOL-Configuration/m-p/1488716#M9548</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;As described in PN7160 Datasheet, 11.2.2.2 SPI-bus configuration options:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;In order to select SPI-bus interface for host communication, some EEPROM settings are&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;programmed during production.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Four versions can be configured depending on CPOL/CPHA EEPROM setting.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The selection between interfaces is fused during IC manufacturing so that different&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ordering numbers for the SPI-bus version.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I have not found any information on different ordernumbers that affect the settings.&lt;BR /&gt;Is this an error?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 11:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160B-CPOL-Configuration/m-p/1488716#M9548</guid>
      <dc:creator>michael_d_1983</dc:creator>
      <dc:date>2022-07-13T11:08:12Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160B - CPOL Configuration</title>
      <link>https://community.nxp.com/t5/NFC/PN7160B-CPOL-Configuration/m-p/1498858#M9572</link>
      <description>&lt;P&gt;I think only I2C vs SPI is programmed during manufacturing. Part number ending with "A" is I2C and "B" is SPI. Clock polarity can be changed later&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 13:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160B-CPOL-Configuration/m-p/1498858#M9572</guid>
      <dc:creator>Erklei</dc:creator>
      <dc:date>2022-08-01T13:45:39Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160B - CPOL Configuration</title>
      <link>https://community.nxp.com/t5/NFC/PN7160B-CPOL-Configuration/m-p/1500380#M9579</link>
      <description>&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;Hello sir,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Unfortunately, the datasheet needs an update. The PN7160 is configured as follows:&lt;/P&gt;
&lt;P&gt;&lt;U&gt;&lt;SPAN class="uiOutputText"&gt;CPHA=0&lt;/SPAN&gt;&lt;/U&gt;&lt;/P&gt;
&lt;P&gt;&lt;U&gt;&lt;SPAN class="uiOutputText"&gt;IFSEL1=0&lt;/SPAN&gt;&lt;/U&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;I hope this information may have been useful.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 16:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160B-CPOL-Configuration/m-p/1500380#M9579</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2022-08-03T16:12:19Z</dc:date>
    </item>
  </channel>
</rss>