<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NT3H2111 FD Pin in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1484819#M9522</link>
    <description>&lt;P&gt;I think the signal is bouncing because the phone is in the near proximity, this is natural and the signal will be stable once you have enough field strength.&lt;/P&gt;&lt;P&gt;You have to debounce the signal in your end with software, as you should do with all noisy signals, such as switches and buttons.&lt;/P&gt;</description>
    <pubDate>Tue, 05 Jul 2022 18:01:25 GMT</pubDate>
    <dc:creator>MrMax</dc:creator>
    <dc:date>2022-07-05T18:01:25Z</dc:date>
    <item>
      <title>NT3H2111 FD Pin</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087499#M7484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) I set FDOn= 00b and FDOff= 00b in NC register of the session bytes of NT3H2111 to catch the RF present or not event. However, I can observe some bouncing signal on FD pin, as attached, when I put a phone near to the NFC antenna. Would you help how to solve the bouncing signal on FD pin? Any register settings in the NT3H2111 can help to solve this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) If the NT3H2111 set to use pass-through,&lt;/P&gt;&lt;P&gt;( i) Will the FD pin go low if a phone put near to the NT3H2111 to read the tag data?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;( ii) Will the FD pin go low if a phone put near to the NT3H2111 to write data to the NT3H2111?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Is there another way except using the pass-through method to acknowledge the microcontroller to read the tag data if a phone put near to write data to the NT3H2111?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 11:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087499#M7484</guid>
      <dc:creator>dt_t</dc:creator>
      <dc:date>2020-06-11T11:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 FD Pin</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087500#M7485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dt.t"&gt;dt.t&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope you are doing well. Are you using a Pull-Up Resistor? Please see the Figure 12 of the &lt;A href="https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf"&gt;Data Sheet&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding your second question, please see this &lt;A href="https://www.nxp.com/docs/en/application-note/AN11579.pdf"&gt;Application Note&lt;/A&gt;, in section 4.1 and 4.2, is the explanation of a Data Transfer from NFC to I2C and from I2C to NFC respectively. The Communication scheme would be really helpful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Field Detection Pin can be configured to react in the following ways:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112855i41B0999B33EE3421/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, if you need your MCU knows when your phone writes to the tag, it is necessary to use the Pass-Through Mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps. If you have any question please let me know.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo Zamora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2020 18:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087500#M7485</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-06-15T18:35:11Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 FD Pin</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087501#M7486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo&lt;/P&gt;&lt;P&gt;Response to your question, I put a 12k pull-up resistor on FD pin. Is&amp;nbsp;it appropriate?&lt;/P&gt;&lt;P&gt;Is the bouncing signal related to the improper matching of the NFC antenna?&lt;/P&gt;&lt;P&gt;Can I put a capacitor on FD pin to the GND to improve the bouncing signal problem? If yes, what values would you advise?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;dt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 01:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087501#M7486</guid>
      <dc:creator>dt_t</dc:creator>
      <dc:date>2020-06-16T01:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 FD Pin</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087502#M7487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about pass-through.&lt;/P&gt;&lt;P&gt;Conditions: PTHRU_ON_OFF= 1b, FD_ON= 11b, FD_OFF=11b, TRANSFER_DIR= 1b( NFC-&amp;gt;I2C)&lt;/P&gt;&lt;P&gt;Does SRAM_I2C_READY set to 1 if NFC try to write data( not longer than 30 bytes) to NT3H2111?&lt;/P&gt;&lt;P&gt;How does microcontroller know the data in SRAM is ready when NFC finish to write the data&lt;SPAN&gt;( not longer than 30 bytes)&lt;/SPAN&gt; to the tag?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;dt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 07:41:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087502#M7487</guid>
      <dc:creator>dt_t</dc:creator>
      <dc:date>2020-06-17T07:41:30Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 FD Pin</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087503#M7488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dt.t"&gt;dt.t&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, that resistor is good. A capacitor should not be necessary.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are two commands: the WRITE command (4 bytes), and the FAST_WRITE command (the 64 bytes of the SRAM). Please refer to the section 4.1 of the &lt;A href="https://www.nxp.com/docs/en/application-note/AN11579.pdf"&gt;Application Note&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The ways the MCU can know the data is ready to be read are:&lt;/P&gt;&lt;UL type="disc"&gt;&lt;LI&gt;The host polls/reads bit SRAM_I2C_READY from NS_REG to know if data is ready in SRAM&lt;/LI&gt;&lt;LI&gt;A trigger on the FD pin indicates to the host that data is ready to be read from SRAM.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 18:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1087503#M7488</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-06-18T18:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 FD Pin</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1484819#M9522</link>
      <description>&lt;P&gt;I think the signal is bouncing because the phone is in the near proximity, this is natural and the signal will be stable once you have enough field strength.&lt;/P&gt;&lt;P&gt;You have to debounce the signal in your end with software, as you should do with all noisy signals, such as switches and buttons.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jul 2022 18:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-FD-Pin/m-p/1484819#M9522</guid>
      <dc:creator>MrMax</dc:creator>
      <dc:date>2022-07-05T18:01:25Z</dc:date>
    </item>
  </channel>
</rss>