<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックProgram/flash PN7462 without MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/NFC/Program-flash-PN7462-without-MCUXpresso-IDE/m-p/1460112#M9438</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I have developed a firmware for the PN7462 microcontroller. I have been using MCUXpresso IDE with LPC-Link 2 to program the firmware. However, this method would be tedious for production porposes. Is there a simpler way to flash the binary without using MCUXpresso IDE? A command line tool would be nice, since it allows us to automate the process using test Jigs.&lt;/P&gt;&lt;P&gt;I want something like the ST's STM32CubeProgrammer, which has both graphical and command line interfaces just to manage ST microcontrollers memory through a ST-Link device.&lt;/P&gt;</description>
    <pubDate>Wed, 18 May 2022 14:47:07 GMT</pubDate>
    <dc:creator>lucasj</dc:creator>
    <dc:date>2022-05-18T14:47:07Z</dc:date>
    <item>
      <title>Program/flash PN7462 without MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/NFC/Program-flash-PN7462-without-MCUXpresso-IDE/m-p/1460112#M9438</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I have developed a firmware for the PN7462 microcontroller. I have been using MCUXpresso IDE with LPC-Link 2 to program the firmware. However, this method would be tedious for production porposes. Is there a simpler way to flash the binary without using MCUXpresso IDE? A command line tool would be nice, since it allows us to automate the process using test Jigs.&lt;/P&gt;&lt;P&gt;I want something like the ST's STM32CubeProgrammer, which has both graphical and command line interfaces just to manage ST microcontrollers memory through a ST-Link device.&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 14:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Program-flash-PN7462-without-MCUXpresso-IDE/m-p/1460112#M9438</guid>
      <dc:creator>lucasj</dc:creator>
      <dc:date>2022-05-18T14:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: Program/flash PN7462 without MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/NFC/Program-flash-PN7462-without-MCUXpresso-IDE/m-p/1460422#M9439</link>
      <description>&lt;P&gt;Hi Lucas:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can use jlink or flash magic.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.flashmagictool.com/" target="_blank"&gt;https://www.flashmagictool.com/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 May 2022 01:12:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Program-flash-PN7462-without-MCUXpresso-IDE/m-p/1460422#M9439</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-05-19T01:12:39Z</dc:date>
    </item>
  </channel>
</rss>