<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: What is the difference between static lock bytes and dynamic lock byte</title>
    <link>https://community.nxp.com/t5/NFC/What-is-the-difference-between-static-lock-bytes-and-dynamic/m-p/612709#M942</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zhaoyu Zhang:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The setting of the dynamic lock bytes is also irreversible, so you can set the bits to 1 but not back to 0. The difference between "static" and "dynamic" is the position in memory for such bits:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;Static&lt;/STRONG&gt; lock bytes are always the bytes 2 and 3 in page 2 of the NTAG memory:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7486i3BE68927C2EAE522/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;Dynamic&lt;/STRONG&gt; lock bytes can be at different positions in memory. For example for NTAG213/215/216 you find the dynamic lock bytes at pages 40/130/226:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7543i8B24362E00DAC603/image-size/large?v=v2&amp;amp;px=999" title="Dynamic_lock.jpg" alt="Dynamic_lock.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This naming is based on the NFC Forum &lt;STRONG&gt;Type 2 Tag&lt;/STRONG&gt; &lt;STRONG&gt;Technical Specification&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Nov 2016 23:21:17 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-11-07T23:21:17Z</dc:date>
    <item>
      <title>What is the difference between static lock bytes and dynamic lock byte</title>
      <link>https://community.nxp.com/t5/NFC/What-is-the-difference-between-static-lock-bytes-and-dynamic/m-p/612708#M941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Taking NTAG 216 for example, I understood that static lock bytes are OTP bytes. While, for dynamic lock bytes, through my experiment, I found &amp;nbsp;that&amp;nbsp;&amp;nbsp;I cannot change them back to 0 either. But this is not mentioned in the spec &amp;nbsp;&lt;A class="link-titled" href="http://www.nxp.com/documents/data_sheet/NTAG213_215_216.pdf" title="http://www.nxp.com/documents/data_sheet/NTAG213_215_216.pdf"&gt;http://www.nxp.com/documents/data_sheet/NTAG213_215_216.pdf&lt;/A&gt;&amp;nbsp;. &amp;nbsp;So just wanted to confirm:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Are dynamic lock bytes also OTP bytes? Or is there a way to change them back to 0 once they are set to 1?&lt;/P&gt;&lt;P&gt;2. If dynamic lock bytes also OTP bytes, then what is the difference between static and dynamic lock bytes except that they lock different address. Basically I don't&amp;nbsp;understand the meaning of &amp;nbsp;'static' and 'dynamic'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Oct 2016 05:13:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/What-is-the-difference-between-static-lock-bytes-and-dynamic/m-p/612708#M941</guid>
      <dc:creator>zhaoyuzhang</dc:creator>
      <dc:date>2016-10-30T05:13:51Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference between static lock bytes and dynamic lock byte</title>
      <link>https://community.nxp.com/t5/NFC/What-is-the-difference-between-static-lock-bytes-and-dynamic/m-p/612709#M942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zhaoyu Zhang:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The setting of the dynamic lock bytes is also irreversible, so you can set the bits to 1 but not back to 0. The difference between "static" and "dynamic" is the position in memory for such bits:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;Static&lt;/STRONG&gt; lock bytes are always the bytes 2 and 3 in page 2 of the NTAG memory:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7486i3BE68927C2EAE522/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;Dynamic&lt;/STRONG&gt; lock bytes can be at different positions in memory. For example for NTAG213/215/216 you find the dynamic lock bytes at pages 40/130/226:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7543i8B24362E00DAC603/image-size/large?v=v2&amp;amp;px=999" title="Dynamic_lock.jpg" alt="Dynamic_lock.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This naming is based on the NFC Forum &lt;STRONG&gt;Type 2 Tag&lt;/STRONG&gt; &lt;STRONG&gt;Technical Specification&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Nov 2016 23:21:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/What-is-the-difference-between-static-lock-bytes-and-dynamic/m-p/612709#M942</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-11-07T23:21:17Z</dc:date>
    </item>
    <item>
      <title>Re: What is the difference between static lock bytes and dynamic lock byte</title>
      <link>https://community.nxp.com/t5/NFC/What-is-the-difference-between-static-lock-bytes-and-dynamic/m-p/612710#M943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for late reply and thanks a lot for the detailed clarification! This is really helpful!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Zhaoyu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2017 19:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/What-is-the-difference-between-static-lock-bytes-and-dynamic/m-p/612710#M943</guid>
      <dc:creator>zhaoyuzhang</dc:creator>
      <dc:date>2017-02-10T19:30:46Z</dc:date>
    </item>
  </channel>
</rss>