<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NFC Antenna Crossing in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1443359#M9355</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank you for the quick reply. It was very helpful.&lt;BR /&gt;&lt;BR /&gt;I'm aware about the tiles and their function.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I've always tended to use the standalone exe NFC Antenna Tool you used to provide. Is the online version better than the standalone one? The only difference i see is the addition of the d&lt;SPAN&gt;ielectric field.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 13 Apr 2022 10:42:24 GMT</pubDate>
    <dc:creator>nike9307</dc:creator>
    <dc:date>2022-04-13T10:42:24Z</dc:date>
    <item>
      <title>NFC Antenna Crossing</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1442772#M9343</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;I was looking at some NXP dev kits and noticed something curious.&lt;BR /&gt;Some kits (like on the PN5180 and the&amp;nbsp;&lt;SPAN&gt;CLRC663) have a antenna that is crossed on the "far" end of the antenna. As far as possible compared to the input signals on the connectors.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Far_end.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176655iA8C8FC761B4478DF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Far_end.jpg" alt="Far_end.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Far_end.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The PN5190 dev kit has the antenna crossing on the near end.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Near_end.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176656iFB1AEBF87BF6BFC0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Near_end.jpg" alt="Near_end.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Near_end.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Does it have any effect on the field. If yes, what are the ups and downs of each design?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Apr 2022 13:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1442772#M9343</guid>
      <dc:creator>nike9307</dc:creator>
      <dc:date>2022-04-12T13:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Antenna Crossing</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1443251#M9353</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196960"&gt;@nike9307&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Indeed the difference is between even or odd number of turns.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;The target is to make the coil as symmetrical as possible. so the PCB layout style for PN5180/CLRC663 kev kit is recommended , but in fact the overall impact is minor.&lt;/P&gt;
&lt;P&gt;Please be aware NOT to copy the copper tiles inside the antenna area: those copper tiles are made only to “emulate” a bad antenna, and must not be copied!&lt;/P&gt;
&lt;P&gt;We also provide a ready to use NFC antenna dev kit, you may refer to&amp;nbsp;&lt;A href="https://www.nxp.com/part/OM29263ADK#/" target="_blank"&gt;https://www.nxp.com/part/OM29263ADK#/&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regarding a good number of turns, please refer to our NFC antenna tool -&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NFC/bd-p/nfc" target="_blank"&gt;https://community.nxp.com/t5/NFC/bd-p/nfc&lt;/A&gt;&amp;nbsp;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Apr 2022 08:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1443251#M9353</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-04-13T08:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Antenna Crossing</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1443359#M9355</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank you for the quick reply. It was very helpful.&lt;BR /&gt;&lt;BR /&gt;I'm aware about the tiles and their function.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I've always tended to use the standalone exe NFC Antenna Tool you used to provide. Is the online version better than the standalone one? The only difference i see is the addition of the d&lt;SPAN&gt;ielectric field.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Apr 2022 10:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1443359#M9355</guid>
      <dc:creator>nike9307</dc:creator>
      <dc:date>2022-04-13T10:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Antenna Crossing</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1443888#M9358</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196960"&gt;@nike9307&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, the online version is the latest.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 14 Apr 2022 07:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Antenna-Crossing/m-p/1443888#M9358</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-04-14T07:33:33Z</dc:date>
    </item>
  </channel>
</rss>