<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with PN5180 firmware 4.0 and DPC enabled. in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Problem-with-PN5180-firmware-4-0-and-DPC-enabled/m-p/1432492#M9282</link>
    <description>&lt;P&gt;But we are running the same tests with the chips already received with firmware 4.0 not upgraded by us to 4.0 so I believe all DPC settings are already adopted to this firmware.&lt;/P&gt;&lt;P&gt;Anything else to check ?&lt;/P&gt;</description>
    <pubDate>Wed, 23 Mar 2022 09:02:06 GMT</pubDate>
    <dc:creator>marcinbaliniak</dc:creator>
    <dc:date>2022-03-23T09:02:06Z</dc:date>
    <item>
      <title>Problem with PN5180 firmware 4.0 and DPC enabled.</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-PN5180-firmware-4-0-and-DPC-enabled/m-p/1394801#M9093</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Recently we did some soak test on our products.&lt;/P&gt;&lt;P&gt;Basically, procedure looks like this:&lt;BR /&gt;11:58:28.630 - Get tag count req...&lt;BR /&gt;11:58:28.725 - TAG is found: 04DA044A5C6684&lt;BR /&gt;11:58:28.725 - Writing random value to page 5 - this is phalMful_Write()&lt;BR /&gt;11:58:28.949 - Reading test page - this is phalMful_Read()&lt;BR /&gt;11:58:28.965 - Read page OK&lt;BR /&gt;11:58:28.965 - Write test passed&lt;BR /&gt;11:58:28.981 - HALT done&lt;/P&gt;&lt;P&gt;This is repeated 3000 times.&lt;/P&gt;&lt;P&gt;And this procedure on the PN5180 firmware 3.5 is fine - 0 errors. But when we use the same procedure on board with PN5180 running firmware 4.0 we have some errors when writing or reading - mostly 0x0203 (PH_COMP_PAL_ISO14443P3A + PH_ERR_COLLISION_ERROR) or 0x0201 (PH_COMP_PAL_ISO14443P3A + PH_ERR_IO_TIMEOUT) - about 30 errors for 3000 cycles of test above.&lt;/P&gt;&lt;P&gt;What we found already when changing EEPROM settings to disable DPC (writing value 0x00 to register 0x59, other EEPROM values left as default) the problem disappears.&lt;/P&gt;&lt;P&gt;NPXLib we are using is 5.12. We know that we can upgrade NXPLib but I don't know if something related to this problem was reported or fixed.&lt;/P&gt;&lt;P&gt;Can you suggest any other than DPC solution to this problem? DPC is a nice feature and we want to keep it on our products.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Marcin.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 11:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-PN5180-firmware-4-0-and-DPC-enabled/m-p/1394801#M9093</guid>
      <dc:creator>marcinbaliniak</dc:creator>
      <dc:date>2022-01-05T11:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with PN5180 firmware 4.0 and DPC enabled.</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-PN5180-firmware-4-0-and-DPC-enabled/m-p/1402978#M9127</link>
      <description>&lt;P&gt;Hi Marcin:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would suggest you check the differences between version 3.5 and version 4.0.&lt;/P&gt;
&lt;P&gt;The differences are listed on PN5180 datasheet.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_0-1642731786817.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168435iD9B45C474F3F2C72/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielchen_0-1642731786817.png" alt="danielchen_0-1642731786817.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If some parameters modified , and you can use cockpit to adjust the relevant settings.&lt;/P&gt;
&lt;P&gt;Here is an application note about dynamic power control.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11742.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11742.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 02:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-PN5180-firmware-4-0-and-DPC-enabled/m-p/1402978#M9127</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-01-21T02:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with PN5180 firmware 4.0 and DPC enabled.</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-PN5180-firmware-4-0-and-DPC-enabled/m-p/1432492#M9282</link>
      <description>&lt;P&gt;But we are running the same tests with the chips already received with firmware 4.0 not upgraded by us to 4.0 so I believe all DPC settings are already adopted to this firmware.&lt;/P&gt;&lt;P&gt;Anything else to check ?&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 09:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-PN5180-firmware-4-0-and-DPC-enabled/m-p/1432492#M9282</guid>
      <dc:creator>marcinbaliniak</dc:creator>
      <dc:date>2022-03-23T09:02:06Z</dc:date>
    </item>
  </channel>
</rss>