<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CLRC663+ MIFARE Classic Authentication issue in NFC</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1425932#M9240</link>
    <description>&lt;P&gt;We have a custom board with CLRC663+ that we use for reading and writing of both MIFARE Classic transponders and MIFARE DESFire EV1 / EV2 transponders.&lt;/P&gt;&lt;P&gt;We have run into an issue with making a MIFARE Classic authentication where the key is 6 x FF (Default key) - The authentication process times out.&lt;/P&gt;&lt;P&gt;Authenticating with non default keys works and the following read or write is successfull.&lt;/P&gt;&lt;P&gt;MIFARE DESFire Auth, Read, Write etc. works too.&lt;/P&gt;&lt;P&gt;Could we be facing a power delivery issue between antenna and card/tag ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Søren Bang&lt;/P&gt;&lt;P&gt;Security Engineering&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Mar 2022 07:52:12 GMT</pubDate>
    <dc:creator>sb2</dc:creator>
    <dc:date>2022-03-10T07:52:12Z</dc:date>
    <item>
      <title>CLRC663+ MIFARE Classic Authentication issue</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1425932#M9240</link>
      <description>&lt;P&gt;We have a custom board with CLRC663+ that we use for reading and writing of both MIFARE Classic transponders and MIFARE DESFire EV1 / EV2 transponders.&lt;/P&gt;&lt;P&gt;We have run into an issue with making a MIFARE Classic authentication where the key is 6 x FF (Default key) - The authentication process times out.&lt;/P&gt;&lt;P&gt;Authenticating with non default keys works and the following read or write is successfull.&lt;/P&gt;&lt;P&gt;MIFARE DESFire Auth, Read, Write etc. works too.&lt;/P&gt;&lt;P&gt;Could we be facing a power delivery issue between antenna and card/tag ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Søren Bang&lt;/P&gt;&lt;P&gt;Security Engineering&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 07:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1425932#M9240</guid>
      <dc:creator>sb2</dc:creator>
      <dc:date>2022-03-10T07:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663+ MIFARE Classic Authentication issue</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1426484#M9241</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/108591"&gt;@sb2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is your application based on NFC reader library? If yes, have you ever tried the demo of "NfcrdlibEx4_MIFAREClassic_mcux" with your Mifare Classic cards? Is the problem still there? Please kindly clarify.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 02:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1426484#M9241</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-03-11T02:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663+ MIFARE Classic Authentication issue</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1426699#M9242</link>
      <description>&lt;P&gt;Dear Kan Li&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for quick reply.&lt;/P&gt;&lt;P&gt;Our current implementation is not based on the NFC reader library as I found it to be to convoluted, so I have rewritten the interface for the CLRC663+.&lt;/P&gt;&lt;P&gt;We are using the CLRC663+ in to different products, but with the same code for interfacing to the CLRC663+. The one product is working fine (5V power supply) and the other product is having the MIFARE Classic Auth issue (3v3 power supply).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Søren&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 07:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1426699#M9242</guid>
      <dc:creator>sb2</dc:creator>
      <dc:date>2022-03-11T07:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663+ MIFARE Classic Authentication issue</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1426717#M9243</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/108591"&gt;@sb2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the clarification! If the same code can work with TVDD=5V but failed at TVDD=3.3V, it is most likely related with the antenna design, what is the target impedance of your antenna design, maybe you have to tune it to a lower value, please also note&amp;nbsp;CLRC663 plus allows an impedance of &amp;lt; 20Ω with the limit of ITVDD = 350 mA.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 08:01:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-MIFARE-Classic-Authentication-issue/m-p/1426717#M9243</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-03-11T08:01:53Z</dc:date>
    </item>
  </channel>
</rss>