<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ask for Blue board p2p project Andoird code in NFC</title>
    <link>https://community.nxp.com/t5/NFC/ask-for-Blue-board-p2p-project-Andoird-code/m-p/611520#M923</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dongmei，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; For CRLRC663, we don't remmend you use it on android platform, if you want to use NFC on android, PN7150 or PN7120 can be selected, because android SDK support them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you insist on applying CLRC663 on android, you will have to do porting by yourself, here is a thought I provide to you:&lt;/P&gt;&lt;P&gt;(1) Hardware connections &amp;amp; drivers(Using SPI&amp;nbsp; )&lt;/P&gt;&lt;P&gt;If using SPI, CLR663 will drived as SPI device by spidev.c in linux dev path. In spidev.c, you will have to provide interfaces for upper level( such as , read, write, lseek, ioctrl function etc for operating CLRC663)&lt;/P&gt;&lt;P&gt;(2)Writing your own API based on C language.&lt;/P&gt;&lt;P&gt;You should write some API functions by interfaces in spidev.c to realize general operations for CLRC663.&lt;/P&gt;&lt;P&gt;(3) SDK for Java&lt;/P&gt;&lt;P&gt;In order to load APIs, you will have to convert APIs based on C to JAVA via android NDK. After this, you will have a set of JAVA SDK for CLRC663&lt;/P&gt;&lt;P&gt;(4) Writing android application by your own SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note, if you use UART interface, porting will be very simple, becuase you only need to operate UART to communicate with CLRC663.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope above advice can help you!&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;TIC Weidong Sun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Apr 2017 04:27:22 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2017-04-26T04:27:22Z</dc:date>
    <item>
      <title>ask for Blue board p2p project Andoird code</title>
      <link>https://community.nxp.com/t5/NFC/ask-for-Blue-board-p2p-project-Andoird-code/m-p/611519#M922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I got the download link of Blue board p2p project from document AM11367 《How to build a NFC Application on Android》CLEV663B [3], but when I opened it, there was no project resource there. Can you send the Blue board p2p project Android code to me? Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Apr 2017 02:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/ask-for-Blue-board-p2p-project-Andoird-code/m-p/611519#M922</guid>
      <dc:creator>mable_one</dc:creator>
      <dc:date>2017-04-14T02:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: ask for Blue board p2p project Andoird code</title>
      <link>https://community.nxp.com/t5/NFC/ask-for-Blue-board-p2p-project-Andoird-code/m-p/611520#M923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dongmei，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; For CRLRC663, we don't remmend you use it on android platform, if you want to use NFC on android, PN7150 or PN7120 can be selected, because android SDK support them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you insist on applying CLRC663 on android, you will have to do porting by yourself, here is a thought I provide to you:&lt;/P&gt;&lt;P&gt;(1) Hardware connections &amp;amp; drivers(Using SPI&amp;nbsp; )&lt;/P&gt;&lt;P&gt;If using SPI, CLR663 will drived as SPI device by spidev.c in linux dev path. In spidev.c, you will have to provide interfaces for upper level( such as , read, write, lseek, ioctrl function etc for operating CLRC663)&lt;/P&gt;&lt;P&gt;(2)Writing your own API based on C language.&lt;/P&gt;&lt;P&gt;You should write some API functions by interfaces in spidev.c to realize general operations for CLRC663.&lt;/P&gt;&lt;P&gt;(3) SDK for Java&lt;/P&gt;&lt;P&gt;In order to load APIs, you will have to convert APIs based on C to JAVA via android NDK. After this, you will have a set of JAVA SDK for CLRC663&lt;/P&gt;&lt;P&gt;(4) Writing android application by your own SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note, if you use UART interface, porting will be very simple, becuase you only need to operate UART to communicate with CLRC663.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope above advice can help you!&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;TIC Weidong Sun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Apr 2017 04:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/ask-for-Blue-board-p2p-project-Andoird-code/m-p/611520#M923</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-04-26T04:27:22Z</dc:date>
    </item>
  </channel>
</rss>