<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: CLRC663 Commands</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1417808#M9217</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191831"&gt;@mgaschler&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the late response and due to I can't get the feedback from the related team.&lt;/P&gt;
&lt;P&gt;But you may refer to the&amp;nbsp;Example Code - Inventory - ISO 15693 of the AN12657 and there is helpful for your application.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;PS: RC663 is working via SPI in the AN.&amp;nbsp; It is just the difference with the communication.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 23 Feb 2022 02:11:54 GMT</pubDate>
    <dc:creator>fangfang</dc:creator>
    <dc:date>2022-02-23T02:11:54Z</dc:date>
    <item>
      <title>CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1413953#M9189</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there an example for using the CLRC663 commands to read an ISO15693 tag? I am able to successfully access the CLRC663 registers over I2C but am looking for a guide on how to configure the registers and which commands to use to successfully read a tag as it appears that many of them need to be adjusted. I would just like to read the UID of the tag. Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Feb 2022 22:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1413953#M9189</guid>
      <dc:creator>mgaschler</dc:creator>
      <dc:date>2022-02-15T22:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414064#M9190</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191831"&gt;@mgaschler&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can refer to the information as the attachment.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 03:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414064#M9190</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2022-02-16T03:19:52Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414564#M9193</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/5061"&gt;@fangfang&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for the reply. I have a few questions:&lt;/P&gt;&lt;P&gt;1. What is the .jcf file?&lt;/P&gt;&lt;P&gt;2. When I try to run the attached script in Cockpit, I get the following error: &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CockpitError.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/170781iF6B1C72EA562ABEB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CockpitError.png" alt="CockpitError.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Do you know why this may be happening?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 16:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414564#M9193</guid>
      <dc:creator>mgaschler</dc:creator>
      <dc:date>2022-02-16T16:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414614#M9196</link>
      <description>&lt;P&gt;Have you managed to configure the NFCRdLIb to work over I2C, and could you share how this was done?&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 17:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414614#M9196</guid>
      <dc:creator>gredpath</dc:creator>
      <dc:date>2022-02-16T17:21:57Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414618#M9197</link>
      <description>&lt;P&gt;I am using U-Boot to communicate with the CLRC663 on the CLEV6630B development board. Some modifications to the board were necessary in order to enable I2C, but otherwise it was pretty straightforward hardware-wise.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 17:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414618#M9197</guid>
      <dc:creator>mgaschler</dc:creator>
      <dc:date>2022-02-16T17:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414655#M9198</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/5061"&gt;@fangfang&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I believe I found the issue with the above error. It looks like line 72 was missing a colon and should have been:&lt;/P&gt;&lt;P&gt;:L_WaitTransceiveFinished&lt;BR /&gt;ReadRegister IRQ1_REG $test&lt;BR /&gt;JumpIfBitN $test 0x40 :L_WaitTransceiveFinished&lt;/P&gt;&lt;P&gt;When I made the change, I no longer get the error. However, now my Cockpit crashes when it reaches this part of the code. After doing some testing, I discovered it was because the value of IRQ1_REG is 0x43, not 0x40, so it gets stuck in an infinite loop. Do you know how I can fix this? If I change the 0x40 value to 0x43, it fixes the infinite loop problem but then I receive no data in the FIFO when trying to read an NFC tag. Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 18:26:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1414655#M9198</guid>
      <dc:creator>mgaschler</dc:creator>
      <dc:date>2022-02-16T18:26:20Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1416090#M9205</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/5061"&gt;@fangfang&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Do you have any ideas about what I said above? Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Feb 2022 15:30:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1416090#M9205</guid>
      <dc:creator>mgaschler</dc:creator>
      <dc:date>2022-02-18T15:30:22Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1417808#M9217</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191831"&gt;@mgaschler&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the late response and due to I can't get the feedback from the related team.&lt;/P&gt;
&lt;P&gt;But you may refer to the&amp;nbsp;Example Code - Inventory - ISO 15693 of the AN12657 and there is helpful for your application.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;PS: RC663 is working via SPI in the AN.&amp;nbsp; It is just the difference with the communication.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 23 Feb 2022 02:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1417808#M9217</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2022-02-23T02:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1419338#M9221</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/5061"&gt;@fangfang&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;AN12657 was exactly what I was looking for! By following the example code and setting the registers using I2C, I was able to read tags successfully. Thank you so much for your help!&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 19:48:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1419338#M9221</guid>
      <dc:creator>mgaschler</dc:creator>
      <dc:date>2022-02-24T19:48:30Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Commands</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1491001#M9563</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can you please tell&amp;nbsp; me that the examples given in&amp;nbsp; AN12657 doc can read tags from smartphones as well or it can only read passive tags?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;Sandeep pawar&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 10:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Commands/m-p/1491001#M9563</guid>
      <dc:creator>Sandeep_Pawar</dc:creator>
      <dc:date>2022-07-18T10:40:51Z</dc:date>
    </item>
  </channel>
</rss>