<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックom2ntp5332</title>
    <link>https://community.nxp.com/t5/NFC/om2ntp5332/m-p/1409666#M9160</link>
    <description>&lt;P&gt;Hi technical support,&lt;/P&gt;&lt;P&gt;Please could you answer the following if possible?&lt;/P&gt;&lt;P&gt;&lt;FONT face="inherit"&gt;&amp;nbsp;I am using the&amp;nbsp;om2ntp5332 NFC evaluation board with the NXP explorer &lt;/FONT&gt;Android&lt;FONT face="inherit"&gt;&amp;nbsp;application. This board is a newer revision Arduino compatible. So the circuit lay out is different to the previous boards.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="inherit"&gt;The question is the intergrated circuit pin out for the&amp;nbsp;om2ntp5332 is the same. So I should be able to monitor the GPIO for a PWM or on of signal. However nothing is happening with the board. The NFC on the application will recordnise the board and report the device ID and memory etc. It will indicate polling and it will activate. However there are no signals on the GPIO pins. Could you please explain what it is. Doing wrong&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="inherit"&gt;Kind regards&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 07 Feb 2022 12:36:57 GMT</pubDate>
    <dc:creator>Steve_buyerh</dc:creator>
    <dc:date>2022-02-07T12:36:57Z</dc:date>
    <item>
      <title>om2ntp5332</title>
      <link>https://community.nxp.com/t5/NFC/om2ntp5332/m-p/1409666#M9160</link>
      <description>&lt;P&gt;Hi technical support,&lt;/P&gt;&lt;P&gt;Please could you answer the following if possible?&lt;/P&gt;&lt;P&gt;&lt;FONT face="inherit"&gt;&amp;nbsp;I am using the&amp;nbsp;om2ntp5332 NFC evaluation board with the NXP explorer &lt;/FONT&gt;Android&lt;FONT face="inherit"&gt;&amp;nbsp;application. This board is a newer revision Arduino compatible. So the circuit lay out is different to the previous boards.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="inherit"&gt;The question is the intergrated circuit pin out for the&amp;nbsp;om2ntp5332 is the same. So I should be able to monitor the GPIO for a PWM or on of signal. However nothing is happening with the board. The NFC on the application will recordnise the board and report the device ID and memory etc. It will indicate polling and it will activate. However there are no signals on the GPIO pins. Could you please explain what it is. Doing wrong&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="inherit"&gt;Kind regards&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 12:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/om2ntp5332/m-p/1409666#M9160</guid>
      <dc:creator>Steve_buyerh</dc:creator>
      <dc:date>2022-02-07T12:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: om2ntp5332</title>
      <link>https://community.nxp.com/t5/NFC/om2ntp5332/m-p/1421008#M9227</link>
      <description>&lt;P&gt;Hi Steve:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I tested with&amp;nbsp;&lt;FONT face="inherit"&gt;NXP explorer&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;SPAN&gt;Android&lt;/SPAN&gt;&lt;FONT face="inherit"&gt;&amp;nbsp;application on&amp;nbsp;&lt;SPAN&gt;om2ntp5332 NFC evaluation board and FRDM-KW41Z board.&amp;nbsp; It can work on my side.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;I configured SW6 to 3.3V. It only connects voltage&amp;nbsp; from underlaying board or source to the NTAG5 and whole PCB.&lt;/P&gt;
&lt;P&gt;If you need to enable energy harvesting, please configure SW3 3-4 to ON position.&lt;/P&gt;
&lt;P&gt;Please refer to RM00230:&amp;nbsp; NTAG 5 link and switch development board -Getting started guide.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/reference-manual/RM00230.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/reference-manual/RM00230.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 01 Mar 2022 07:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/om2ntp5332/m-p/1421008#M9227</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-03-01T07:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: om2ntp5332</title>
      <link>https://community.nxp.com/t5/NFC/om2ntp5332/m-p/1451335#M9410</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Is it possible to receive the project you used to help Steve? Currently, you are replying to a thread of mine in which I am trying to connect the KW41Z and the om2ntp5332 to realise pass-through functionality alongside energy harvesting.&lt;/P&gt;&lt;P&gt;Thanks for your reply,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stefan Cremers&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 12:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/om2ntp5332/m-p/1451335#M9410</guid>
      <dc:creator>StefanC</dc:creator>
      <dc:date>2022-04-29T12:31:00Z</dc:date>
    </item>
  </channel>
</rss>