<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 PN7462 Using GPIO14 as GPIO Output?</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-Using-GPIO14-as-GPIO-Output/m-p/1390212#M9072</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;How can I configure GPIO14(CLK_AUX) as GPIO output and set it's value?&lt;/P&gt;&lt;P&gt;I know I should use "ph_Reg.h" file but couldn't find out what should i do exactly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 21 Dec 2021 14:48:19 GMT</pubDate>
    <dc:creator>EE_Ark</dc:creator>
    <dc:date>2021-12-21T14:48:19Z</dc:date>
    <item>
      <title>PN7462 Using GPIO14 as GPIO Output?</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Using-GPIO14-as-GPIO-Output/m-p/1390212#M9072</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;How can I configure GPIO14(CLK_AUX) as GPIO output and set it's value?&lt;/P&gt;&lt;P&gt;I know I should use "ph_Reg.h" file but couldn't find out what should i do exactly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Dec 2021 14:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Using-GPIO14-as-GPIO-Output/m-p/1390212#M9072</guid>
      <dc:creator>EE_Ark</dc:creator>
      <dc:date>2021-12-21T14:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Using GPIO14 as GPIO Output?</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Using-GPIO14-as-GPIO-Output/m-p/1390676#M9075</link>
      <description>&lt;P&gt;I tried these codes without success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PH_REG_SET_BITN(PCR_PAD_CLK_AUX_REG,PCR_PAD_CLK_AUX_REG_CLK_AUX_GPIOMODE_EN_POS);&lt;/P&gt;&lt;P&gt;//PH_REG_SET_FIELD( PCR_PAD_CLK_AUX_REG , CLK_AUX_PUPD,0x2);//pull up&lt;BR /&gt;//PH_REG_SET_FIELD( PCR_PAD_CLK_AUX_REG , CLK_AUX_PUPD,0x3);//pull down&lt;/P&gt;&lt;P&gt;PH_REG_SET_BIT(PCR_PADOUT_REG,PADOUT_CLK_AUX); //Set CLK_AUX HIGH&lt;BR /&gt;PH_REG_CLEAR_BIT(PCR_PADOUT_REG,PADOUT_CLK_AUX);&amp;nbsp;//Set CLK_AUX LOW&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 08:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Using-GPIO14-as-GPIO-Output/m-p/1390676#M9075</guid>
      <dc:creator>EE_Ark</dc:creator>
      <dc:date>2021-12-22T08:58:12Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Using GPIO14 as GPIO Output?</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Using-GPIO14-as-GPIO-Output/m-p/1391451#M9080</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193309"&gt;@EE_Ark&lt;/a&gt;&amp;nbsp;:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In order to config GPIO output,&amp;nbsp; you can try API:&amp;nbsp;phhalPcr_ConfigOutput&amp;nbsp; () and&amp;nbsp;PH_HAL_GPIO_SETGPIOVAL ()&lt;/P&gt;
&lt;P&gt;You can refer to pphhalPcr_GpioInit() function in phhalGpio.c&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Dec 2021 16:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Using-GPIO14-as-GPIO-Output/m-p/1391451#M9080</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2021-12-23T16:18:31Z</dc:date>
    </item>
  </channel>
</rss>