<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: SL3S40X1 Read Protection</title>
    <link>https://community.nxp.com/t5/NFC/SL3S40X1-Read-Protection/m-p/1375191#M9011</link>
    <description>&lt;P&gt;When read protect is enabled the IC will only allow this information to be read when in the “secured” state. However, the I²C interface always has this “secured” privilege. Please check this in section 12&amp;nbsp;RF interface/I2C interface arbitration.&lt;/P&gt;&lt;P&gt;"I2C access to the chip memory is possible regardless if it is in the EPC Gen2 secured&lt;BR /&gt;state or not"&lt;/P&gt;&lt;P&gt;This means that whenever you need to disable the UCODE memory protection you can do this securely by I2C.&lt;/P&gt;</description>
    <pubDate>Mon, 22 Nov 2021 19:12:01 GMT</pubDate>
    <dc:creator>Fabian_R</dc:creator>
    <dc:date>2021-11-22T19:12:01Z</dc:date>
    <item>
      <title>SL3S40X1 Read Protection</title>
      <link>https://community.nxp.com/t5/NFC/SL3S40X1-Read-Protection/m-p/1370010#M8994</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'd like to know what are the SL3S40X1 capabilities for user memory protection. After reading the datasheet, I still have following questions:&lt;/P&gt;&lt;P&gt;- After activation of the read protection, the user memory cannot be read via: RF, I2C or both?&lt;/P&gt;&lt;P&gt;- How could this read protection be disabled?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Thu, 11 Nov 2021 14:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/SL3S40X1-Read-Protection/m-p/1370010#M8994</guid>
      <dc:creator>MCU_0X55</dc:creator>
      <dc:date>2021-11-11T14:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: SL3S40X1 Read Protection</title>
      <link>https://community.nxp.com/t5/NFC/SL3S40X1-Read-Protection/m-p/1375191#M9011</link>
      <description>&lt;P&gt;When read protect is enabled the IC will only allow this information to be read when in the “secured” state. However, the I²C interface always has this “secured” privilege. Please check this in section 12&amp;nbsp;RF interface/I2C interface arbitration.&lt;/P&gt;&lt;P&gt;"I2C access to the chip memory is possible regardless if it is in the EPC Gen2 secured&lt;BR /&gt;state or not"&lt;/P&gt;&lt;P&gt;This means that whenever you need to disable the UCODE memory protection you can do this securely by I2C.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Nov 2021 19:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/SL3S40X1-Read-Protection/m-p/1375191#M9011</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2021-11-22T19:12:01Z</dc:date>
    </item>
  </channel>
</rss>