<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7462: Register for current DPC Gear in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-Register-for-current-DPC-Gear/m-p/1358577#M8943</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;were are currently developing an application using the PN7462 with 4 DPC gears. Is it possible to read the current gear from a register (when the field is active of course)?&lt;/P&gt;&lt;P&gt;The NFC cockpit has the desired function implemented, but I don't have any clue how to read it within the C application based on the Reader-Lib.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="johannesdev_0-1634726570415.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/159626i7DEE7D82DB768789/image-size/large?v=v2&amp;amp;px=999" role="button" title="johannesdev_0-1634726570415.png" alt="johannesdev_0-1634726570415.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;BR /&gt;Johannes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Oct 2021 10:48:57 GMT</pubDate>
    <dc:creator>johannesdev</dc:creator>
    <dc:date>2021-10-20T10:48:57Z</dc:date>
    <item>
      <title>PN7462: Register for current DPC Gear</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Register-for-current-DPC-Gear/m-p/1358577#M8943</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;were are currently developing an application using the PN7462 with 4 DPC gears. Is it possible to read the current gear from a register (when the field is active of course)?&lt;/P&gt;&lt;P&gt;The NFC cockpit has the desired function implemented, but I don't have any clue how to read it within the C application based on the Reader-Lib.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="johannesdev_0-1634726570415.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/159626i7DEE7D82DB768789/image-size/large?v=v2&amp;amp;px=999" role="button" title="johannesdev_0-1634726570415.png" alt="johannesdev_0-1634726570415.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;BR /&gt;Johannes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 10:48:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Register-for-current-DPC-Gear/m-p/1358577#M8943</guid>
      <dc:creator>johannesdev</dc:creator>
      <dc:date>2021-10-20T10:48:57Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462: Register for current DPC Gear</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Register-for-current-DPC-Gear/m-p/1362331#M8958</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/146905"&gt;@johannesdev&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may have the current AGC value from the following register.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1635326371946.png" style="width: 596px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160386i0E6D044AA0034259/image-dimensions/596x224?v=v2" width="596" height="224" role="button" title="Kan_Li_0-1635326371946.png" alt="Kan_Li_0-1635326371946.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;but have to calculate the current gear number with help of high/low AGC threshold for each gear, as well as the gear size, gear step size and start gear number. Please kindly refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN11742.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11742.pdf&lt;/A&gt; for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that makes sense,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 09:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Register-for-current-DPC-Gear/m-p/1362331#M8958</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-10-27T09:23:22Z</dc:date>
    </item>
  </channel>
</rss>