<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NFC security using PN5180 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NFC-security-using-PN5180/m-p/1352734#M8916</link>
    <description>&lt;P&gt;Hi, I am new to NFC technology and was wondering how secure different MIFARE cards are nowadays. There are different kinds of cards like: MIFARE Classic, MIFARE UltraLight and MIFARE DESFire. I am interested in developing a NFC reader to identify people using NFC card technology. It is of utmost importance that no clones of a certain card can be made and the data can’t be read by malicious people since this setup is to be used as an access control system. I am a bit in the dark about how to start, where to start, which technology/security to use, which data must be stored. I have planned to develop an application using Zephyr RTOS for the IMXRT1064 which is connected with a PN5180. In the datasheet of the PN5180 I don’t seem to find a lot about security except for `MIFARE_AUTHENTICATE`. (Is this very secure?) Does this mean that the PN5180 limits me to use MIFARE Classic since it doesn’t seem to support MIFARE DESFIRE, or is this a wrong assumption. Thanks in advance&lt;/P&gt;</description>
    <pubDate>Fri, 08 Oct 2021 13:50:17 GMT</pubDate>
    <dc:creator>Matthias-A</dc:creator>
    <dc:date>2021-10-08T13:50:17Z</dc:date>
    <item>
      <title>NFC security using PN5180</title>
      <link>https://community.nxp.com/t5/NFC/NFC-security-using-PN5180/m-p/1352734#M8916</link>
      <description>&lt;P&gt;Hi, I am new to NFC technology and was wondering how secure different MIFARE cards are nowadays. There are different kinds of cards like: MIFARE Classic, MIFARE UltraLight and MIFARE DESFire. I am interested in developing a NFC reader to identify people using NFC card technology. It is of utmost importance that no clones of a certain card can be made and the data can’t be read by malicious people since this setup is to be used as an access control system. I am a bit in the dark about how to start, where to start, which technology/security to use, which data must be stored. I have planned to develop an application using Zephyr RTOS for the IMXRT1064 which is connected with a PN5180. In the datasheet of the PN5180 I don’t seem to find a lot about security except for `MIFARE_AUTHENTICATE`. (Is this very secure?) Does this mean that the PN5180 limits me to use MIFARE Classic since it doesn’t seem to support MIFARE DESFIRE, or is this a wrong assumption. Thanks in advance&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 13:50:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-security-using-PN5180/m-p/1352734#M8916</guid>
      <dc:creator>Matthias-A</dc:creator>
      <dc:date>2021-10-08T13:50:17Z</dc:date>
    </item>
    <item>
      <title>Re: NFC security using PN5180</title>
      <link>https://community.nxp.com/t5/NFC/NFC-security-using-PN5180/m-p/1353805#M8920</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;PN5180 can support MIFARE&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;DESFIRE and there is the library for the customer. But the library is under NDA.&amp;nbsp; So you need an NDA to gain access to that documentation. If you has&amp;nbsp; NDA. Please refer to the attachment how to find the document on Docstore.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 02:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-security-using-PN5180/m-p/1353805#M8920</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-10-12T02:26:23Z</dc:date>
    </item>
  </channel>
</rss>