<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN532 TransportData Questions</title>
    <link>https://community.nxp.com/t5/NFC/PN532-TransportData-Questions/m-p/1335576#M8824</link>
    <description>&lt;P&gt;I know that PN532 is a transferable byte 262byte, but 64byte is sent when it is sent in P2P Initiator mode. How do I send more than 64 bytes?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Perhaps it is because the value of LRi in ATR_REQ is 00 and only 64byte data is checked. How can I change this value?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 06 Sep 2021 15:35:57 GMT</pubDate>
    <dc:creator>kimhyungjun</dc:creator>
    <dc:date>2021-09-06T15:35:57Z</dc:date>
    <item>
      <title>PN532 TransportData Questions</title>
      <link>https://community.nxp.com/t5/NFC/PN532-TransportData-Questions/m-p/1335576#M8824</link>
      <description>&lt;P&gt;I know that PN532 is a transferable byte 262byte, but 64byte is sent when it is sent in P2P Initiator mode. How do I send more than 64 bytes?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Perhaps it is because the value of LRi in ATR_REQ is 00 and only 64byte data is checked. How can I change this value?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Sep 2021 15:35:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN532-TransportData-Questions/m-p/1335576#M8824</guid>
      <dc:creator>kimhyungjun</dc:creator>
      <dc:date>2021-09-06T15:35:57Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 TransportData Questions</title>
      <link>https://community.nxp.com/t5/NFC/PN532-TransportData-Questions/m-p/1336722#M8825</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189266"&gt;@kimhyungjun&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The command of&amp;nbsp;InDataExchange can be used for that purpose, and there is an example in&amp;nbsp;Fig 103., please refer to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/141520.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/141520.pdf&lt;/A&gt;&amp;nbsp;for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 08:38:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN532-TransportData-Questions/m-p/1336722#M8825</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-09-08T08:38:34Z</dc:date>
    </item>
  </channel>
</rss>