<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Write NT3H2211 NFC Command timing tACK in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Write-NT3H2211-NFC-Command-timing-tACK/m-p/1329297#M8800</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;When I use WRITE or FAST WRITE command NFC in order to write a page in NT3H2211 eeprom, how much time is the tACK time ( please see datasheet at page 55 ) ?&lt;/P&gt;&lt;P&gt;As the eeprom write is 4,7ms long, will I receive the ack of the write command after these 4,7ms or before?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In other words, when I receive an ack from the NFC write command sent by my app, am I sure that the data is correctlly written in the eeprom or no?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 25 Aug 2021 08:48:24 GMT</pubDate>
    <dc:creator>gb31</dc:creator>
    <dc:date>2021-08-25T08:48:24Z</dc:date>
    <item>
      <title>Write NT3H2211 NFC Command timing tACK</title>
      <link>https://community.nxp.com/t5/NFC/Write-NT3H2211-NFC-Command-timing-tACK/m-p/1329297#M8800</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;When I use WRITE or FAST WRITE command NFC in order to write a page in NT3H2211 eeprom, how much time is the tACK time ( please see datasheet at page 55 ) ?&lt;/P&gt;&lt;P&gt;As the eeprom write is 4,7ms long, will I receive the ack of the write command after these 4,7ms or before?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In other words, when I receive an ack from the NFC write command sent by my app, am I sure that the data is correctlly written in the eeprom or no?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 08:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Write-NT3H2211-NFC-Command-timing-tACK/m-p/1329297#M8800</guid>
      <dc:creator>gb31</dc:creator>
      <dc:date>2021-08-25T08:48:24Z</dc:date>
    </item>
    <item>
      <title>Re: Write NT3H2211 NFC Command timing tACK</title>
      <link>https://community.nxp.com/t5/NFC/Write-NT3H2211-NFC-Command-timing-tACK/m-p/1329899#M8804</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;
&lt;P&gt;Please refer to the&amp;nbsp;10.2 Timing of the datasheet. And for the more information please refer to&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. NFC Forum - Type 2 Tag Specification 1.0&lt;BR /&gt;Technical Specification&lt;BR /&gt;2. ISO/IEC 14443 - Identification cards - Contactless integrated circuit cards - Proximity&lt;BR /&gt;cards&lt;BR /&gt;International Standard.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you! &lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 02:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Write-NT3H2211-NFC-Command-timing-tACK/m-p/1329899#M8804</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-08-26T02:05:51Z</dc:date>
    </item>
  </channel>
</rss>