<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックCannot write to ISO15693 NFC tags using CLEV663 Development board</title>
    <link>https://community.nxp.com/t5/NFC/Cannot-write-to-ISO15693-NFC-tags-using-CLEV663-Development/m-p/1328621#M8790</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a few Tag-It NFC cards (using ISO15693) from Texas instruments which were encoded by another manufacturer. I would like to use the same cards in parallel for my application too. To do this, I will require to write to some sectors of the NFC card memory.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My setup consists of a CLEV663 board which is controller by the NXP NFC Cockpit v5.9 and a few Tag-It cards.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can perform all the read operations but I cannot write to NFC cards. Below is a list of the commands I executed and the response from the card;&lt;/P&gt;&lt;P&gt;Get System Information: Command: 0x2B, Flags: 0x12, Response:&amp;nbsp;: SUCCESS, Data: 0F6B8AE52A000007E000003F038B&lt;/P&gt;&lt;P&gt;Get Multiple Block Security Status Blocks 0 and 1: Command: 0x2C0001, Flags: 0x12 Response:&amp;nbsp;SUCCESS, Data: 0000&lt;/P&gt;&lt;P&gt;Read Block 1: Command: 0x2001, Flags: 0x12, Response:&amp;nbsp;00000000&lt;/P&gt;&lt;P&gt;Write Block 1 with data 0x33221100:&amp;nbsp;Command: 0x210100112233, Flags: 0x52, Response: ERROR:RFProtocolType15693Service:Perform15693DataExchangeFailed: PAL_SLI15693,ISO15693&lt;/P&gt;&lt;P&gt;Even though the block security is not set, I cannot write to it. Can somebody please help?&lt;/P&gt;</description>
    <pubDate>Tue, 24 Aug 2021 11:54:26 GMT</pubDate>
    <dc:creator>software_memo</dc:creator>
    <dc:date>2021-08-24T11:54:26Z</dc:date>
    <item>
      <title>Cannot write to ISO15693 NFC tags using CLEV663 Development board</title>
      <link>https://community.nxp.com/t5/NFC/Cannot-write-to-ISO15693-NFC-tags-using-CLEV663-Development/m-p/1328621#M8790</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a few Tag-It NFC cards (using ISO15693) from Texas instruments which were encoded by another manufacturer. I would like to use the same cards in parallel for my application too. To do this, I will require to write to some sectors of the NFC card memory.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My setup consists of a CLEV663 board which is controller by the NXP NFC Cockpit v5.9 and a few Tag-It cards.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can perform all the read operations but I cannot write to NFC cards. Below is a list of the commands I executed and the response from the card;&lt;/P&gt;&lt;P&gt;Get System Information: Command: 0x2B, Flags: 0x12, Response:&amp;nbsp;: SUCCESS, Data: 0F6B8AE52A000007E000003F038B&lt;/P&gt;&lt;P&gt;Get Multiple Block Security Status Blocks 0 and 1: Command: 0x2C0001, Flags: 0x12 Response:&amp;nbsp;SUCCESS, Data: 0000&lt;/P&gt;&lt;P&gt;Read Block 1: Command: 0x2001, Flags: 0x12, Response:&amp;nbsp;00000000&lt;/P&gt;&lt;P&gt;Write Block 1 with data 0x33221100:&amp;nbsp;Command: 0x210100112233, Flags: 0x52, Response: ERROR:RFProtocolType15693Service:Perform15693DataExchangeFailed: PAL_SLI15693,ISO15693&lt;/P&gt;&lt;P&gt;Even though the block security is not set, I cannot write to it. Can somebody please help?&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 11:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Cannot-write-to-ISO15693-NFC-tags-using-CLEV663-Development/m-p/1328621#M8790</guid>
      <dc:creator>software_memo</dc:creator>
      <dc:date>2021-08-24T11:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot write to ISO15693 NFC tags using CLEV663 Development board</title>
      <link>https://community.nxp.com/t5/NFC/Cannot-write-to-ISO15693-NFC-tags-using-CLEV663-Development/m-p/1329125#M8796</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Actually Cockpit is designed for hardware test purpose, and usually used for the antenna design and optimization, and we provide NFC reader library for custom application, this library includes the example for&amp;nbsp; ISO15693 as the link.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY" target="_blank"&gt;https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you! &lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 05:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Cannot-write-to-ISO15693-NFC-tags-using-CLEV663-Development/m-p/1329125#M8796</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-08-25T05:48:55Z</dc:date>
    </item>
  </channel>
</rss>