<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CLRC663 T0 underflow and T0COUNTERVAL register does not keep values in NFC</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-T0-underflow-and-T0COUNTERVAL-register-does-not-keep/m-p/1325081#M8780</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;One may refer to the code as the link.&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/how-to-communicate-between-LPC1769-and-RC663-via-SPI-based-on/ta-p/1303617" target="_blank"&gt;https://community.nxp.com/t5/NFC-Knowledge-Base/how-to-communicate-between-LPC1769-and-RC663-via-SPI-based-on/ta-p/1303617&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;It is SPI communication .But the application can meet your requirement.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you! &lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 18 Aug 2021 02:20:35 GMT</pubDate>
    <dc:creator>fangfang</dc:creator>
    <dc:date>2021-08-18T02:20:35Z</dc:date>
    <item>
      <title>CLRC663 T0 underflow and T0COUNTERVAL register does not keep values</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-T0-underflow-and-T0COUNTERVAL-register-does-not-keep/m-p/1324879#M8778</link>
      <description>&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on a project in which I&amp;nbsp; use a CLRC663 for NFC communication with type 2 tags. I use this library that I adapted for the RS232 communication protocol ( I just defined write_reg and read_reg functions) : &lt;A title="CLRC663 Lib" href="https://github.com/kenny5660/CLRC663" target="_blank" rel="noopener"&gt;https://github.com/kenny5660/CLRC663&amp;nbsp;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;When I try to read/ write registers as Version register or command register all works as it should. However, when I try to send the REQA protocole, I have T0 underflow IRQ and when I try to change the value in T0COUNTERVAL[HI/LO] registers nothing change and the CLRC answer me that the 2 registers are at 0x00 when I read them.&lt;/P&gt;&lt;P&gt;As initialisation I use &lt;EM&gt;CLRC663_AN1102_recommended_registers(CLRC663_PROTO_ISO14443A_106_MILLER_MANCHESTER); &lt;/EM&gt;function and I do my REQA after.&lt;/P&gt;&lt;P&gt;Do you have some ideas to help me with this problem ?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mathieu&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 16:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-T0-underflow-and-T0COUNTERVAL-register-does-not-keep/m-p/1324879#M8778</guid>
      <dc:creator>M_Chene</dc:creator>
      <dc:date>2021-08-17T16:36:33Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 T0 underflow and T0COUNTERVAL register does not keep values</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-T0-underflow-and-T0COUNTERVAL-register-does-not-keep/m-p/1325081#M8780</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;One may refer to the code as the link.&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/how-to-communicate-between-LPC1769-and-RC663-via-SPI-based-on/ta-p/1303617" target="_blank"&gt;https://community.nxp.com/t5/NFC-Knowledge-Base/how-to-communicate-between-LPC1769-and-RC663-via-SPI-based-on/ta-p/1303617&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;It is SPI communication .But the application can meet your requirement.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you! &lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 02:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-T0-underflow-and-T0COUNTERVAL-register-does-not-keep/m-p/1325081#M8780</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-08-18T02:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 T0 underflow and T0COUNTERVAL register does not keep values</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-T0-underflow-and-T0COUNTERVAL-register-does-not-keep/m-p/1499708#M9577</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am developing a similar product on a microcontroller different from NXP, and the whole library is very hard to integrate and very poorly documented&lt;/P&gt;&lt;P&gt;Would you like to get in touch?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Write me at &lt;A href="mailto:cgaudiolaboratories.cg2@gmail.com" target="_blank"&gt;cgaudiolaboratories.cg2@gmail.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Bye&lt;/P&gt;&lt;P&gt;CG&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 15:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-T0-underflow-and-T0COUNTERVAL-register-does-not-keep/m-p/1499708#M9577</guid>
      <dc:creator>lcenni</dc:creator>
      <dc:date>2022-08-02T15:46:09Z</dc:date>
    </item>
  </channel>
</rss>