<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN5180 and wrong value of RX_STATUS register in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN5180-and-wrong-value-of-RX-STATUS-register/m-p/1323479#M8776</link>
    <description>&lt;P&gt;Hello. I have a board with a PN5180 chip, ordered on Aliexpress (for &lt;A href="https://a.aliexpress.com/_mNGtk5z" target="_self"&gt;&lt;FONT face="batang,apple gothic"&gt;example&lt;/FONT&gt;&lt;/A&gt;). I have the following problem.&lt;/P&gt;&lt;P&gt;When I sending the RATS command to PICC, the RX_STATUS register displays an incomplete number of returned bytes. It can be 0x05, 0x07, 0x0A, when the correct value is 0x13.&lt;/P&gt;&lt;P&gt;During the experiment, I noticed that if you leave a pause for a few milliseconds before starting the RX_STATUS register reading function and only then read the register, the correct number of bytes received will return - 0x13.&lt;/P&gt;&lt;P&gt;I notice this behavior only in commands to which PICC returns long responses. That is, the correct value will be returned by RX_STATUS to the ATQA command both with and without a pause, and the correct number of bytes will be returned to the RATS command only after a pause.&lt;/P&gt;&lt;P&gt;It turns out that the chip does not process the data immediately after receiving it and it needs time to process them? Then how can I track the state of readiness for reading the RX_STATUS register and data?&lt;/P&gt;&lt;P&gt;Maybe this can be found using another register, for example, IRQ_STATUS? Maybe the developers of the PN5180 have accurate data about how long the pause should last for the chip to have time to process the data?&lt;/P&gt;&lt;P&gt;If you need clarification on my question, please specify. I need a solution that is based on the requirements of the chip, and not on some random guesses, because I need the maximum performance of the chip.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Sat, 14 Aug 2021 21:34:40 GMT</pubDate>
    <dc:creator>Unknown0</dc:creator>
    <dc:date>2021-08-14T21:34:40Z</dc:date>
    <item>
      <title>PN5180 and wrong value of RX_STATUS register</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-and-wrong-value-of-RX-STATUS-register/m-p/1323479#M8776</link>
      <description>&lt;P&gt;Hello. I have a board with a PN5180 chip, ordered on Aliexpress (for &lt;A href="https://a.aliexpress.com/_mNGtk5z" target="_self"&gt;&lt;FONT face="batang,apple gothic"&gt;example&lt;/FONT&gt;&lt;/A&gt;). I have the following problem.&lt;/P&gt;&lt;P&gt;When I sending the RATS command to PICC, the RX_STATUS register displays an incomplete number of returned bytes. It can be 0x05, 0x07, 0x0A, when the correct value is 0x13.&lt;/P&gt;&lt;P&gt;During the experiment, I noticed that if you leave a pause for a few milliseconds before starting the RX_STATUS register reading function and only then read the register, the correct number of bytes received will return - 0x13.&lt;/P&gt;&lt;P&gt;I notice this behavior only in commands to which PICC returns long responses. That is, the correct value will be returned by RX_STATUS to the ATQA command both with and without a pause, and the correct number of bytes will be returned to the RATS command only after a pause.&lt;/P&gt;&lt;P&gt;It turns out that the chip does not process the data immediately after receiving it and it needs time to process them? Then how can I track the state of readiness for reading the RX_STATUS register and data?&lt;/P&gt;&lt;P&gt;Maybe this can be found using another register, for example, IRQ_STATUS? Maybe the developers of the PN5180 have accurate data about how long the pause should last for the chip to have time to process the data?&lt;/P&gt;&lt;P&gt;If you need clarification on my question, please specify. I need a solution that is based on the requirements of the chip, and not on some random guesses, because I need the maximum performance of the chip.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Sat, 14 Aug 2021 21:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-and-wrong-value-of-RX-STATUS-register/m-p/1323479#M8776</guid>
      <dc:creator>Unknown0</dc:creator>
      <dc:date>2021-08-14T21:34:40Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 and wrong value of RX_STATUS register</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-and-wrong-value-of-RX-STATUS-register/m-p/1327082#M8785</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Hello, my name is Fabian, I've been assigned to support your case.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Thank you for your interest in our products.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Unfortunately, the support provided by us is limited to our boards. My apologies for the problems this may cause.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;I encourage you to please check our PN5180 &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/full-nfc-forum-compliant-frontend-ic:PN5180?&amp;amp;tab=Documentation_Tab&amp;amp;linkline=Data-Sheet" target="_blank"&gt;Datasheet &lt;/A&gt;and start working with the manufacturer of the board you bought.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 19:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-and-wrong-value-of-RX-STATUS-register/m-p/1327082#M8785</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2021-08-20T19:03:49Z</dc:date>
    </item>
  </channel>
</rss>