<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN7150 LPCUSBSIO</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-LPCUSBSIO/m-p/1315066#M8723</link>
    <description>&lt;P&gt;Any help with this?&lt;/P&gt;</description>
    <pubDate>Thu, 29 Jul 2021 06:54:24 GMT</pubDate>
    <dc:creator>matthew5025</dc:creator>
    <dc:date>2021-07-29T06:54:24Z</dc:date>
    <item>
      <title>PN7150 LPCUSBSIO</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-LPCUSBSIO/m-p/1309501#M8695</link>
      <description>&lt;P&gt;When using the&amp;nbsp;linux_libnfc-nci with LPCUSBSIO as described &lt;A href="https://www.nxp.com/docs/en/application-note/AN11697.pdf" target="_self"&gt;here&lt;/A&gt;, there seems to be an issue with Card Emulation. Sending a large response to the reader (~200 bytes) seems to cause the library to lock up and no longer process any other commands.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;This does not occur when using the library in alt mode, nor when using the code provided in &lt;A href="https://www.nxp.com/doc/SW4335" target="_self"&gt;SW4335&lt;/A&gt;, so it seems to be specific to the&amp;nbsp;linux_libnfc-nci with LPCUSBSIO combination.&lt;/P&gt;&lt;P&gt;I've attached some logs in a GitHub issue (&lt;A href="https://github.com/NXPNFCLinux/linux_libnfc-nci/issues/133" target="_blank"&gt;https://github.com/NXPNFCLinux/linux_libnfc-nci/issues/133&lt;/A&gt;)&lt;BR /&gt;&lt;BR /&gt;Is this a known limitation, or is there a workaround for this issue?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 03:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-LPCUSBSIO/m-p/1309501#M8695</guid>
      <dc:creator>matthew5025</dc:creator>
      <dc:date>2021-07-19T03:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 LPCUSBSIO</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-LPCUSBSIO/m-p/1315066#M8723</link>
      <description>&lt;P&gt;Any help with this?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 06:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-LPCUSBSIO/m-p/1315066#M8723</guid>
      <dc:creator>matthew5025</dc:creator>
      <dc:date>2021-07-29T06:54:24Z</dc:date>
    </item>
  </channel>
</rss>