<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: InDataExchange response Time</title>
    <link>https://community.nxp.com/t5/NFC/InDataExchange-response-Time/m-p/608367#M857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rishi Franklin:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you measured the difference in time for successful and failed transfers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The timeout extension request is indeed handled by the PN532 as target, but by default it sends a request for a maximum of 1.078s. See the manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13519i65AE93F81724596F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the target should send a response before that time elapses.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Feb 2017 22:15:06 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2017-02-16T22:15:06Z</dc:date>
    <item>
      <title>InDataExchange response Time</title>
      <link>https://community.nxp.com/t5/NFC/InDataExchange-response-Time/m-p/608366#M856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PN532 in P2P mode wherein the sequence of commands on initiator is like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. [Initiator] - InJumpForDep&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. [Initiator] - InDataExchange&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the Target side i have the flow&lt;/P&gt;&lt;P&gt;1. [Target] InitAsTarget&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. TargetRx - [TgGetData]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Perform processing based on data received, (takes time t)&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. TargetTx - [TgSetData]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore when i give the InDataExchange command on Initiator, on target side it uses GetData, Process, SetData.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now then, TgSetData is returning error status as 0x29 - Target released by initiator.&lt;/P&gt;&lt;P&gt;I have observed that when the&amp;nbsp; processing time t is small the status is OK but when t is large&lt;/P&gt;&lt;P&gt;the status is 0x29. Given that i have not procedurally released the target using InRelease, is there&lt;/P&gt;&lt;P&gt;some timeout setting that i am missing ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the data sheet the S(TO)REQ/RES is managed by PN532. I've set the CFgItem02 &amp;amp; 0x05 using RFConfiguration commands to maximum timeout values but then they are only associated with InJumpForDEP/ATR_REQ/RES&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the question is, is there a timeout value associated with InDataExchange ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 06:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/InDataExchange-response-Time/m-p/608366#M856</guid>
      <dc:creator>testbed</dc:creator>
      <dc:date>2017-02-07T06:54:04Z</dc:date>
    </item>
    <item>
      <title>Re: InDataExchange response Time</title>
      <link>https://community.nxp.com/t5/NFC/InDataExchange-response-Time/m-p/608367#M857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rishi Franklin:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you measured the difference in time for successful and failed transfers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The timeout extension request is indeed handled by the PN532 as target, but by default it sends a request for a maximum of 1.078s. See the manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13519i65AE93F81724596F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the target should send a response before that time elapses.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 22:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/InDataExchange-response-Time/m-p/608367#M857</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2017-02-16T22:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: InDataExchange response Time</title>
      <link>https://community.nxp.com/t5/NFC/InDataExchange-response-Time/m-p/608368#M858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jorge, i figured i was setting the 1 sec timeout on target side instead on the initiator cfg registers......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2017 16:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/InDataExchange-response-Time/m-p/608368#M858</guid>
      <dc:creator>testbed</dc:creator>
      <dc:date>2017-02-23T16:49:35Z</dc:date>
    </item>
  </channel>
</rss>