<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックabout the command PWD_AUTH and  config DEV_SEC_CONFIG</title>
    <link>https://community.nxp.com/t5/NFC/about-the-command-PWD-AUTH-and-config-DEV-SEC-CONFIG/m-p/1285825#M8561</link>
    <description>&lt;P&gt;There are two problem：&lt;/P&gt;&lt;P&gt;1.&lt;SPAN&gt;Now I follow all the steps(from 7.1 to 7.5) of example in&amp;nbsp;&amp;nbsp;the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="fontstyle0"&gt;AN12366(this document is Memory configuration and scalable security)&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;,so I set the PWD and restricited area configuration.Then how to use the pwd?Would you explain more about it（I had seen that the command&amp;nbsp;PWD_AUTH was used to&amp;nbsp;authenticate in NTAG I2C,but I can't seen this command in NTAG 5 Link.Why?）&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2.&amp;nbsp;I had bought the board NTP5312.I use the command 12C0043F00 to get the DEV_SEC_CONFIG,but the response is 4500FFFF. 45h means&amp;nbsp;block 3Fh with device security configuration bytes is locked。So I can't set the Restricted area protection pointer (PP_AREA_1).Why?The default configuration of&amp;nbsp;&amp;nbsp;DEV_SEC_CONFIG isn't&amp;nbsp; A500FFFF?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 02 Jun 2021 05:29:08 GMT</pubDate>
    <dc:creator>finecook</dc:creator>
    <dc:date>2021-06-02T05:29:08Z</dc:date>
    <item>
      <title>about the command PWD_AUTH and  config DEV_SEC_CONFIG</title>
      <link>https://community.nxp.com/t5/NFC/about-the-command-PWD-AUTH-and-config-DEV-SEC-CONFIG/m-p/1285825#M8561</link>
      <description>&lt;P&gt;There are two problem：&lt;/P&gt;&lt;P&gt;1.&lt;SPAN&gt;Now I follow all the steps(from 7.1 to 7.5) of example in&amp;nbsp;&amp;nbsp;the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="fontstyle0"&gt;AN12366(this document is Memory configuration and scalable security)&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;,so I set the PWD and restricited area configuration.Then how to use the pwd?Would you explain more about it（I had seen that the command&amp;nbsp;PWD_AUTH was used to&amp;nbsp;authenticate in NTAG I2C,but I can't seen this command in NTAG 5 Link.Why?）&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2.&amp;nbsp;I had bought the board NTP5312.I use the command 12C0043F00 to get the DEV_SEC_CONFIG,but the response is 4500FFFF. 45h means&amp;nbsp;block 3Fh with device security configuration bytes is locked。So I can't set the Restricted area protection pointer (PP_AREA_1).Why?The default configuration of&amp;nbsp;&amp;nbsp;DEV_SEC_CONFIG isn't&amp;nbsp; A500FFFF?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 05:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/about-the-command-PWD-AUTH-and-config-DEV-SEC-CONFIG/m-p/1285825#M8561</guid>
      <dc:creator>finecook</dc:creator>
      <dc:date>2021-06-02T05:29:08Z</dc:date>
    </item>
    <item>
      <title>Re: about the command PWD_AUTH and  config DEV_SEC_CONFIG</title>
      <link>https://community.nxp.com/t5/NFC/about-the-command-PWD-AUTH-and-config-DEV-SEC-CONFIG/m-p/1295611#M8613</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Answering your first question, NTAG I2C is a T2T, and NTAG5 is a T5T, they have different commands, so if you are looking for information about the NTAG 5 Link, please check the &lt;A href="https://www.nxp.com/docs/en/data-sheet/NTP53x2.pdf" target="_blank"&gt;NTAG 5 link Data Sheet&lt;/A&gt; (section 8.2.3 Command set).&lt;/P&gt;
&lt;P&gt;Also, please check section 8.2.3.3 PWD Authentication. There you can find the information of how the tag can be configured to be uses for password authentication.&lt;/P&gt;
&lt;P&gt;About the second question, it looks like at some point you sent a command that protected the tag, this is why it doesn’t have the default configuration.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 19:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/about-the-command-PWD-AUTH-and-config-DEV-SEC-CONFIG/m-p/1295611#M8613</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2021-06-21T19:05:27Z</dc:date>
    </item>
  </channel>
</rss>