<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NTAG213 Counter in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NTAG213-Counter/m-p/1280704#M8538</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any way to increment the NFC counter on power up?&amp;nbsp;&lt;/P&gt;&lt;P&gt;The data sheet shows that the counter will not be incremented until a read or fast read command. Is that correct?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can think of a number of relevant use cases where counter increment on power up without the need for an external read command would be useful.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;</description>
    <pubDate>Sun, 23 May 2021 08:15:03 GMT</pubDate>
    <dc:creator>AW1511</dc:creator>
    <dc:date>2021-05-23T08:15:03Z</dc:date>
    <item>
      <title>NTAG213 Counter</title>
      <link>https://community.nxp.com/t5/NFC/NTAG213-Counter/m-p/1280704#M8538</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any way to increment the NFC counter on power up?&amp;nbsp;&lt;/P&gt;&lt;P&gt;The data sheet shows that the counter will not be incremented until a read or fast read command. Is that correct?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can think of a number of relevant use cases where counter increment on power up without the need for an external read command would be useful.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;</description>
      <pubDate>Sun, 23 May 2021 08:15:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG213-Counter/m-p/1280704#M8538</guid>
      <dc:creator>AW1511</dc:creator>
      <dc:date>2021-05-23T08:15:03Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG213 Counter</title>
      <link>https://community.nxp.com/t5/NFC/NTAG213-Counter/m-p/1283520#M8548</link>
      <description>&lt;P&gt;Is there any update on this counter functionality?&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 13:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG213-Counter/m-p/1283520#M8548</guid>
      <dc:creator>AW1511</dc:creator>
      <dc:date>2021-05-27T13:46:39Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG213 Counter</title>
      <link>https://community.nxp.com/t5/NFC/NTAG213-Counter/m-p/1284312#M8550</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;The NFC counter will be automatically increased at the first READ or FAST_READ command after a power on reset.&lt;/P&gt;
&lt;P&gt;So, the command is necessary to increase the counter value.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 21:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG213-Counter/m-p/1284312#M8550</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2021-05-28T21:45:20Z</dc:date>
    </item>
  </channel>
</rss>