<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7150 c11006</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-c11006/m-p/1278135#M8529</link>
    <description>&lt;P&gt;&lt;SPAN&gt;hi，if the pn7150 hardware VS switch to c11006 from c11002, it is there anything need to modify in the Android system driver? can it be replaced directly?&lt;BR /&gt;thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 18 May 2021 09:32:57 GMT</pubDate>
    <dc:creator>zhichaotan</dc:creator>
    <dc:date>2021-05-18T09:32:57Z</dc:date>
    <item>
      <title>PN7150 c11006</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-c11006/m-p/1278135#M8529</link>
      <description>&lt;P&gt;&lt;SPAN&gt;hi，if the pn7150 hardware VS switch to c11006 from c11002, it is there anything need to modify in the Android system driver? can it be replaced directly?&lt;BR /&gt;thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 09:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-c11006/m-p/1278135#M8529</guid>
      <dc:creator>zhichaotan</dc:creator>
      <dc:date>2021-05-18T09:32:57Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 c11006</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-c11006/m-p/1278532#M8531</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Both version of the difference is just a firmware update and this are backwards compatible,&amp;nbsp; Version C11006 ,&lt;/SPAN&gt;&lt;SPAN&gt;PN7150B0HN/C11006 contains a firmware update compared to the previous version.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The firmware version is 10.01.AE and contains the following new features and fixes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• Anti tearing mechanism: An Anti tearing mechanism has been added. For details,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;please refer to the User Manual UM10936.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;• A fix has been added that addresses a collision resolution problem for ISO 15693 tags&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;in case there are multiple tags in the field.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 02:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-c11006/m-p/1278532#M8531</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-05-19T02:09:58Z</dc:date>
    </item>
  </channel>
</rss>