<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NTAG NT3H2111/ NT3H2211 I²C Communication Problem in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NTAG-NT3H2111-NT3H2211-I-C-Communication-Problem/m-p/1274971#M8515</link>
    <description>&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have solved the problem myself. But maybe someone stumbles across the same problem:&lt;/P&gt;&lt;P&gt;It seems that the NTAG had taken the address 0x00. I didn't know that this is possible as it is usually the broadcast address. Since there is another slave on the bus which is responding on 0x00, I didn't notice it at all.&lt;BR /&gt;So I solved the problem by adressing the slave via the address 0x00 and setting the first register back to default values .&amp;nbsp;Fortunately, the other slave device on the bus was not affected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Tue, 11 May 2021 10:55:57 GMT</pubDate>
    <dc:creator>d_schoenfisch</dc:creator>
    <dc:date>2021-05-11T10:55:57Z</dc:date>
    <item>
      <title>NTAG NT3H2111/ NT3H2211 I²C Communication Problem</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-NT3H2111-NT3H2211-I-C-Communication-Problem/m-p/1274330#M8513</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently using the NTAG I²C plus in some setup with an LPC810 and an I²C ADC.&lt;/P&gt;&lt;P&gt;At the beginning everything worked relatively well, but now I cannot "address" the NTAG via I²C. I had already had the problem with the changed I²C address and solved it successfully (I found it with address 0x2A and reset it to 0x55).&lt;/P&gt;&lt;P&gt;I actually use two "selfmade" test boards and have somehow either misadjusted or "destroyed" the chip on both. I can no longer communicate with the chips via I²C. NFC communication still works on one board, but not on the other.&lt;/P&gt;&lt;P&gt;I use an external voltage source (3V3) to test and program the microcontroller. However, since I ultimately want to operate the setup only via NFC, I have connected the VOUT and VCC pins. Can this lead to problems if I use both, external power supply and read out the chip via NFC at the same time?&lt;/P&gt;&lt;P&gt;I have already scanned through all the I²C addresses to see if they could be wrong again. Unfortunately I don't get an answer for any address (except 0x00 and 0x48 which is from another device on the bus).&lt;/P&gt;&lt;P&gt;I have read out the chip with a working NFC interface. The config registers (0E8 and 0E9) are set to [0x01, 0x00, 0xF8, 0x48] and [0x08, 0x01, 0x00, --]. Which should be OK according to my interpretation.&lt;/P&gt;&lt;P&gt;I also tried to reset the NTAG (the I2C interface) via a "repeated start condition" without a stop condition in between. But I am not sure if I have interpreted the instructions from the data sheet correctly. A picture of the I²C communication is below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My questions in brief:&lt;/P&gt;&lt;P&gt;- Did I do the reset of the I²C interface correctly?&lt;/P&gt;&lt;P&gt;- Is there anything else I can try to reset the NTAG?&lt;/P&gt;&lt;P&gt;- Could I have changed something in Config, that is causing the NTAG to stop working?&lt;/P&gt;&lt;P&gt;- Could it be that I have somehow "destroyed" the chips or the I2C interface because I am using an external voltage source and the harvesting function at the same time?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Repeated start on I²C:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="david_schoenfis_0-1620634408792.png" style="width: 741px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/144339i26315BC19E62D764/image-dimensions/741x91?v=v2" width="741" height="91" role="button" title="david_schoenfis_0-1620634408792.png" alt="david_schoenfis_0-1620634408792.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 May 2021 08:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-NT3H2111-NT3H2211-I-C-Communication-Problem/m-p/1274330#M8513</guid>
      <dc:creator>d_schoenfisch</dc:creator>
      <dc:date>2021-05-10T08:15:46Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG NT3H2111/ NT3H2211 I²C Communication Problem</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-NT3H2111-NT3H2211-I-C-Communication-Problem/m-p/1274971#M8515</link>
      <description>&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have solved the problem myself. But maybe someone stumbles across the same problem:&lt;/P&gt;&lt;P&gt;It seems that the NTAG had taken the address 0x00. I didn't know that this is possible as it is usually the broadcast address. Since there is another slave on the bus which is responding on 0x00, I didn't notice it at all.&lt;BR /&gt;So I solved the problem by adressing the slave via the address 0x00 and setting the first register back to default values .&amp;nbsp;Fortunately, the other slave device on the bus was not affected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Tue, 11 May 2021 10:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-NT3H2111-NT3H2211-I-C-Communication-Problem/m-p/1274971#M8515</guid>
      <dc:creator>d_schoenfisch</dc:creator>
      <dc:date>2021-05-11T10:55:57Z</dc:date>
    </item>
  </channel>
</rss>