<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CT &amp; CLIF Card Operation in NFC</title>
    <link>https://community.nxp.com/t5/NFC/CT-CLIF-Card-Operation/m-p/1272132#M8498</link>
    <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;having the same problem as describe by 'sachin_singh'. could you elaborate how to solve this?&lt;/P&gt;&lt;P&gt;thx in advance&lt;/P&gt;&lt;P&gt;hari&lt;/P&gt;</description>
    <pubDate>Wed, 05 May 2021 10:32:35 GMT</pubDate>
    <dc:creator>hglanzer</dc:creator>
    <dc:date>2021-05-05T10:32:35Z</dc:date>
    <item>
      <title>CT &amp; CLIF Card Operation</title>
      <link>https://community.nxp.com/t5/NFC/CT-CLIF-Card-Operation/m-p/962700#M6122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the PN7462AU card reader with Evaluation kit using PN7462AU-FW_v05.07.01_Full firmware file with "phExCcid" example. Which is for Contact and Contact-less cards detection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to perform the operation on both card when both are present at same time. But yes only one card get the command fired by the user respectlivily.&lt;/P&gt;&lt;P&gt;For example say that, Card reader has both the card Contact and contact-less card present at the same time. When user need to fire command for contact card then it should received by contact card similarly for the contact-less also. (For Contact-less card - MIFARE CLASSIC 1k and contact card - SAM CARD).&lt;/P&gt;&lt;P&gt;In short I need to perform the operation on both cards (contact and contact-less cards) but one at a time in presence to two cards - contact and contact-less cards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, Please kindly guide to achieve these functionality for two card operation on PN7462AU.&lt;/P&gt;&lt;P&gt;If possible then also share the API/data/document/any example related to it.&lt;/P&gt;&lt;P&gt;Your all the support &amp;amp; response are highly appreciative.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward for the supports.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 07:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CT-CLIF-Card-Operation/m-p/962700#M6122</guid>
      <dc:creator>sachin_singh</dc:creator>
      <dc:date>2019-10-09T07:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: CT &amp; CLIF Card Operation</title>
      <link>https://community.nxp.com/t5/NFC/CT-CLIF-Card-Operation/m-p/962701#M6123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A reply was already made to your case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 20:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CT-CLIF-Card-Operation/m-p/962701#M6123</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-10-11T20:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: CT &amp; CLIF Card Operation</title>
      <link>https://community.nxp.com/t5/NFC/CT-CLIF-Card-Operation/m-p/1272132#M8498</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;having the same problem as describe by 'sachin_singh'. could you elaborate how to solve this?&lt;/P&gt;&lt;P&gt;thx in advance&lt;/P&gt;&lt;P&gt;hari&lt;/P&gt;</description>
      <pubDate>Wed, 05 May 2021 10:32:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CT-CLIF-Card-Operation/m-p/1272132#M8498</guid>
      <dc:creator>hglanzer</dc:creator>
      <dc:date>2021-05-05T10:32:35Z</dc:date>
    </item>
  </channel>
</rss>